sl_btmesh_evt_mbt_client_server_transfer_status#

The MBT Server's current transfer status.

This event contains the current transfer status received from a MBT Server. The status is received as a response to sl_btmesh_mbt_client_start_transfer or sl_btmesh_mbt_client_get_transfer_status commands.

Modules#

sl_btmesh_evt_mbt_client_server_transfer_status_s

Macros#

#define

Identifier of the server_transfer_status event.

Typedef Documentation#

sl_btmesh_evt_mbt_client_server_transfer_status_t#

typedef struct sl_btmesh_evt_mbt_client_server_transfer_status_s sl_btmesh_evt_mbt_client_server_transfer_status_t

Definition at line 10428 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_mbt_client_server_transfer_status_id#

#define sl_btmesh_evt_mbt_client_server_transfer_status_id
Value:
0x012800a8

Identifier of the server_transfer_status event.


Definition at line 10406 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h