sl_btmesh_evt_mbt_client_start_transfer_complete#

Transfer start is complete.

All active servers have responded to the transfer start command. The first block start should be initiated with sl_btmesh_mbt_client_start_block.

Modules#

sl_btmesh_evt_mbt_client_start_transfer_complete_s

Macros#

#define
sl_btmesh_evt_mbt_client_start_transfer_complete_id 0x052800a8

Identifier of the start_transfer_complete event.

Typedef Documentation#

sl_btmesh_evt_mbt_client_start_transfer_complete_t#

typedef struct sl_btmesh_evt_mbt_client_start_transfer_complete_s sl_btmesh_evt_mbt_client_start_transfer_complete_t

Definition at line 10452 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h