CommunicationComponents
Description
Host communication interface.
The Communication component provides an interface for implementing communication with a host device, such as a computer or a microcontroller.
Communication Protocol Implementations
Several components implement the communication interface, using different transports and protocols.
Bluetooth Apploader OTA DFU
BGAPI UART DFU
EZSP-SPI
ezsp-spi-bootloader
that was previously released with the EmberZnet and SL-Thread wireless stacks. UART XMODEM
serial-uart-bootloader
that was previously released with the EmberZnet and SL-Thread wireless stacks. Modules | |
Utils | |
Function Documentation
void bootloader_apploader_communication_init | ( | void |
| ) |
Initialize hardware for the BLE Apploader OTA DFU Bootloader communication.
int32_t bootloader_apploader_communication_start | ( | void |
| ) |
Initialize communication between the BLE Apploader OTA DFU bootloader and external host.
- Returns
- Error code indicating success or failure.
int32_t bootloader_apploader_communication_main | ( | ImageProperties_t * | imageProps, |
ParserContext_t * | parserContext, |
||
DecryptContext_t * | decryptContext, |
||
AuthContext_t * | authContext, |
||
const BootloaderParserCallbacks_t * | parseCb |
||
) |
Communication main for the BLE Apploader OTA DFU bootloader.
- Parameters
-
imageProps
The image file processed parserContext
Image parser context decryptContext
Image decryption context authContext
Image authentication context parseCb
Bootloader parser callbacks
- Returns
- Error code indicating success or failure.
void bootloader_bgapi_communication_init | ( | void |
| ) |
Initialize hardware for the BGAPI UART DFU Bootloader communication.
int32_t bootloader_bgapi_communication_start | ( | void |
| ) |
Initialize communication between the BGAPI UART DFU bootloader and external host.
- Returns
- Error code indicating success or failure.
int32_t bootloader_bgapi_communication_main | ( | ImageProperties_t * | imageProps, |
ParserContext_t * | parserContext, |
||
const BootloaderParserCallbacks_t * | parseCb |
||
) |
Communication main for the BGAPI UART DFU bootloader.
- Parameters
-
imageProps
The image file processed parserContext
Image parser context parseCb
Bootloader parser callbacks
- Returns
- Error code indicating success or failure.
void communication_init | ( | void |
| ) |
Initialize hardware for the communication component.
int32_t communication_start | ( | void |
| ) |
Initialize communication between the bootloader and external host. For example, indicate that all is well to the external host.
- Returns
- Error code indicating success or failure
- Return values
-
BOOTLOADER_OK
on success BOOTLOADER_ERROR_COMMUNICATION_START
on failure
int32_t communication_main | ( | void |
| ) |
Not supposed to return until either the host signals the end of the current session or a new image has been flashed and verified.
- Returns
- Error code indicating success or failure
- Return values
-
BOOTLOADER_OK
when a new image was flashed BOOTLOADER_ERROR_COMMUNICATION_ERROR
on communication error BOOTLOADER_ERROR_COMMUNICATION_DONE
when no image was received BOOTLOADER_ERROR_COMMUNICATION_IMAGE_ERROR
when received image is invalid
void communication_shutdown | ( | void |
| ) |
Stop communication between the bootloader and external host.
void bootloader_ezsp_communication_init | ( | void |
| ) |
Initialize hardware for the EZSP SPI Bootloader communication.
int32_t bootloader_ezsp_communication_start | ( | void |
| ) |
Initialize communication between the EZSP SPI bootloader and external host.
- Returns
- Error code indicating success or failure.
int32_t bootloader_ezsp_communication_main | ( | ImageProperties_t * | imageProps, |
ParserContext_t * | parserContext, |
||
const BootloaderParserCallbacks_t * | parseCb |
||
) |
Communication main for the EZSP SPI bootloader.
- Parameters
-
imageProps
The image file processed parserContext
Image parser context parseCb
Bootloader parser callbacks
- Returns
- Error code indicating success or failure.
void bootloader_ezsp_communication_shutdown | ( | void |
| ) |
Stop communication between the bootloader and external host.
void bootloader_xmodem_communication_init | ( | void |
| ) |
Initialize hardware for the UART XMODEM Bootloader communication.
int32_t bootloader_xmodem_communication_start | ( | void |
| ) |
Initialize communication between the UART XMODEM bootloader and external host.
- Returns
- Error code indicating success or failure.
int32_t bootloader_xmodem_communication_main | ( | ImageProperties_t * | imageProps, |
const BootloaderParserCallbacks_t * | parseCb |
||
) |
Communication main for the UART XMODEM bootloader.
- Parameters
-
imageProps
The image file processed parseCb
Bootloader parser callbacks
- Returns
- Error code indicating success or failure.