GblSeUpgrade_t Struct ReferenceComponents > Image Parser > GBL Parser > GBL Format
Description
GBL SE upgrade tag type.
Definition at line 177
of file btl_gbl_format.h
.
#include <
btl_gbl_format.h
>
Data Fields | |
GblTagHeader_t | header |
Tag ID and length. | |
uint32_t | blobSize |
Size of the SE upgrade blob. | |
uint32_t | version |
Version of the SE image. | |
uint8_t * | data |
Array of data for SE upgrade. | |
The documentation for this struct was generated from the following file:
btl_gbl_format.h