ApplicationData Struct ReferenceApplication Interface > Application Properties
Description
Application Data.
Definition at line 95
of file application_properties.h
.
#include <
application_properties.h
>
Data Fields | |
uint32_t | type |
Bitfield representing type of application, e.g., APPLICATION_TYPE_ZIGBEE. | |
uint32_t | version |
Version number for this application. | |
uint32_t | capabilities |
Capabilities of this application. | |
uint8_t | productId [16] |
Unique ID (UUID or GUID) for the product this application is built for. | |
The documentation for this struct was generated from the following file:
application_properties.h