Modules
The following is a list of the different bootloader APIs, both those that are internal to the bootloader, and those available to any application running alongside the bootloader.
▼Application Interface | Application interface to the bootloader |
Application Parser Interface | Application interface for the bootloader image parser |
Application Properties | Properties of the application that can be accessed by the bootloader |
Application Storage Interface | Application interface for interfacing with the bootloader storage |
▼Common Application Interface | Generic application interface available on all versions of the bootloader, regardless of the available components |
Reset Information | Passing information when resetting into and out of the bootloader |
▼Bootloader Core | Core bootloader functionality |
Bootload | Methods to verify and bootload application images |
Flash | Interface to internal flash |
Reset | Methods to reset from the bootloader to the app |
TrustZone | TrustZone utilities |
Upgrade | Methods to verify and upgrade the main bootloader |
▼Components | |
▼Communication | Host communication interface |
▼Utils | |
▼XMODEM Parser | Parser for XMODEM packets |
Commands | |
Debug | Debug Component |
▼Decompressor | Decompressors for Gecko Bootloader |
LZ4 Decompressor | LZ4 decompressor |
▼GPIO Activation | Enter bootloader based on GPIO state |
Button GPIO | Enter bootloader based on Button GPIO state |
EZSP GPIO | Enter bootloader based on EZSP GPIO state |
▼Image Parser | |
▼GBL Parser | GBL parser implementation |
▼Custom GBL Tags | Handle custom GBL tags for added functionality in the GBL parser |
LZ4 Programming Tag | Tag to handle LZ4 compressed programming data |
LZMA Programming Tag | Tag to handle LZMA compressed programming data |
GBL Format | |
▼Security | Collection of security components |
AES | AES decryption functionality for bootloader |
CRC16 | CRC16 functionality for the bootloader |
CRC32 | CRC32 functionality for the bootloader |
Decryption | Generic decryption functionality for bootloader |
▼ECDSA | ECDSA signing functionality for the bootloader |
ECC Library | Elliptic Curve Cryptography Library |
SHA256 | SHA-256 Cryptography Library |
SHA_256 | SHA-256 digest functionality for the bootloader |
Tokens | Manufacturing token handling for the bootloader |
▼Storage | Storage component |
Bootload Info | Indicates which firmware update image should be bootloaded next |
SPI Flash Configurations | Configuration parameters for SPI flashes |
SPI Flash Configurations using SFDP | Configuration parameters for SPI flashes Using JEDEC SFDP Standard |
▼Driver | Hardware drivers for bootloader |
Delay | Basic delay functionality |
SPI | Basic Serial Peripheral Interface Driver |
SPI Peripheral | SPI Peripheral Interface driver |
UART | Serial UART Interface Driver |
▼Error Codes | Bootloader error codes |
Bootloading Error Codes | Bootloader error codes returned by the bootloading process |
Communication Component Error Codes | Bootloader error codes returned by communication components |
Compression Error Codes | Bootloader error codes returned by the decompressor |
Error Code Base Values | Bootloader error code base values, per logical function |
Image Parser Error Codes | Bootloader error codes returned by the image file parser |
Initialization Error Codes | Bootloader error codes returned by initialization code |
Parse Error Codes | Bootloader error codes returned by image parsing |
SPI Peripheral Driver Error Codes | Bootloader error codes returned by the SPI Peripheral driver |
Security Error Codes | Bootloader error codes returned by security algorithms |
Storage Driver Error Codes | Bootloader error codes returned by a storage driver |
UART Driver Error Codes | Bootloader error codes returned by the UART driver |
XMODEM Error Codes | Bootloader error codes returned by the XMODEM parser |