VersionDependency_t Struct ReferenceComponents > Image Parser > GBL Parser > GBL Format
Description
GBL version dependency tag type.
Definition at line
155
of file
btl_gbl_format.h
.
#include <
btl_gbl_format.h
>
Data Fields |
|
| uint8_t | imageType |
|
Type of image (application, bootloader, SE)
|
|
| uint8_t | statement |
|
Encoded dependency statement (ex. appVersion > (0).1.2.3)
|
|
| uint16_t | reserved |
|
Reserved.
|
|
| uint32_t | version |
|
The version number used in the statement (ex. (0).1.2.3)
|
|
The documentation for this struct was generated from the following file:
-
btl_gbl_format.h