XmodemPacket_t Struct ReferenceComponents > Communication > Utils > XMODEM Parser
Description
XMODEM packet.
Definition at line 71
of file btl_xmodem.h
.
#include <
btl_xmodem.h
>
Data Fields | |
uint8_t | header |
Packet header (XMODEM_CMD_SOH) | |
uint8_t | packetNumber |
Packet sequence number. | |
uint8_t | packetNumberC |
Complement of packet sequence number. | |
uint8_t | data [XMODEM_DATA_SIZE] |
Payload. | |
uint8_t | crcH |
CRC high byte. | |
uint8_t | crcL |
CRC low byte. | |
The documentation for this struct was generated from the following file:
btl_xmodem.h