BootloaderStorageFunctions Struct ReferenceApplication Interface > Application Storage Interface

Description

Storage API accessible from the application.

Definition at line 117 of file btl_interface_storage.h.

#include <btl_interface_storage.h>

Data Fields

uint32_t version
 Version of this struct.
 
void(* getInfo )(BootloaderStorageInformation_t *info)
 Get information about the storage – capabilities, layout, configuration.
 
int32_t(* getSlotInfo )(uint32_t slotId, BootloaderStorageSlot_t *slot)
 Get information about storage slot – size, location.
 
int32_t(* read )(uint32_t slotId, uint32_t offset, uint8_t *buffer, size_t length)
 Read bytes from slot into buffer.
 
int32_t(* write )(uint32_t slotId, uint32_t offset, uint8_t *buffer, size_t length)
 Write bytes from buffer into slot.
 
int32_t(* erase )(uint32_t slotId)
 Erase an entire slot.
 
int32_t(* setImagesToBootload )(int32_t *slotIds, size_t length)
 Mark a list of slots for bootload.
 
int32_t(* getImagesToBootload )(int32_t *slotIds, size_t length)
 Mark a list of slots for bootload.
 
int32_t(* appendImageToBootloadList )(int32_t slotId)
 Append a slot to bootload list.
 
int32_t(* initParseImage )(uint32_t slotId, BootloaderParserContext_t *context, size_t contextSize)
 Start image parsing.
 
int32_t(* verifyImage )(BootloaderParserContext_t *context, BootloaderParserCallback_t metadataCallback)
 Continue image verification.
 
int32_t(* getImageInfo )(BootloaderParserContext_t *context, ApplicationData_t *appInfo, uint32_t *bootloaderVersion)
 Get app and bootloader upgrade information from storage slot.
 
bool(* isBusy )(void)
 Check whether the bootloader storage is busy.
 
int32_t(* readRaw )(uint32_t address, uint8_t *buffer, size_t length)
 Read raw bytes from storage.
 
int32_t(* writeRaw )(uint32_t address, uint8_t *buffer, size_t length)
 Write bytes to raw storage.
 
int32_t(* eraseRaw )(uint32_t address, size_t length)
 Erase storage.
 
int32_t(* getDMAchannel )(void)
 Get configured DMA channel.
 

The documentation for this struct was generated from the following file:
  • btl_interface_storage.h