BootloaderInformation_t Struct ReferenceApplication Interface > Common Application Interface
Description
Information about the current bootloader.
Definition at line 105
of file btl_interface.h
.
#include <
btl_interface.h
>
Data Fields | |
BootloaderType_t | type |
The type of bootloader. | |
uint32_t | version |
Version number of the bootloader. | |
uint32_t | capabilities |
Capability mask for the bootloader. | |
The documentation for this struct was generated from the following file:
btl_interface.h