RTCCEMLIB

Detailed Description

Real Time Counter (RTCC) Peripheral API.

This module contains functions to control the RTCC peripheral of Silicon Labs 32-bit MCUs and SoCs. The RTCC ensures timekeeping in low energy modes. The RTCC also includes a BCD calendar mode for easy time and date keeping.

Data Structures

struct  RTCC_CCChConf_TypeDef
 
struct  RTCC_Init_TypeDef
 

Macros

#define RTCC_CH_INIT_CAPTURE_DEFAULT
 
#define RTCC_CH_INIT_COMPARE_DEFAULT
 
#define RTCC_CH_VALID(ch)    ( (ch) < 3)
 
#define RTCC_INIT_DEFAULT
 

Enumerations

enum  RTCC_CapComChMode_TypeDef {
  rtccCapComChModeOff = _RTCC_CC_CTRL_MODE_OFF,
  rtccCapComChModeCapture = _RTCC_CC_CTRL_MODE_INPUTCAPTURE,
  rtccCapComChModeCompare = _RTCC_CC_CTRL_MODE_OUTPUTCOMPARE
}
 
enum  RTCC_CntMode_TypeDef {
  rtccCntModeNormal = _RTCC_CTRL_CNTMODE_NORMAL,
  rtccCntModeCalendar = _RTCC_CTRL_CNTMODE_CALENDAR
}
 
enum  RTCC_CntPresc_TypeDef {
  rtccCntPresc_1 = _RTCC_CTRL_CNTPRESC_DIV1,
  rtccCntPresc_2 = _RTCC_CTRL_CNTPRESC_DIV2,
  rtccCntPresc_4 = _RTCC_CTRL_CNTPRESC_DIV4,
  rtccCntPresc_8 = _RTCC_CTRL_CNTPRESC_DIV8,
  rtccCntPresc_16 = _RTCC_CTRL_CNTPRESC_DIV16,
  rtccCntPresc_32 = _RTCC_CTRL_CNTPRESC_DIV32,
  rtccCntPresc_64 = _RTCC_CTRL_CNTPRESC_DIV64,
  rtccCntPresc_128 = _RTCC_CTRL_CNTPRESC_DIV128,
  rtccCntPresc_256 = _RTCC_CTRL_CNTPRESC_DIV256,
  rtccCntPresc_512 = _RTCC_CTRL_CNTPRESC_DIV512,
  rtccCntPresc_1024 = _RTCC_CTRL_CNTPRESC_DIV1024,
  rtccCntPresc_2048 = _RTCC_CTRL_CNTPRESC_DIV2048,
  rtccCntPresc_4096 = _RTCC_CTRL_CNTPRESC_DIV4096,
  rtccCntPresc_8192 = _RTCC_CTRL_CNTPRESC_DIV8192,
  rtccCntPresc_16384 = _RTCC_CTRL_CNTPRESC_DIV16384,
  rtccCntPresc_32768 = _RTCC_CTRL_CNTPRESC_DIV32768
}
 
enum  RTCC_CompBase_TypeDef {
  rtccCompBaseCnt = _RTCC_CC_CTRL_COMPBASE_CNT,
  rtccCompBasePreCnt = _RTCC_CC_CTRL_COMPBASE_PRECNT
}
 
enum  RTCC_CompMatchOutAction_TypeDef {
  rtccCompMatchOutActionPulse = _RTCC_CC_CTRL_CMOA_PULSE,
  rtccCompMatchOutActionToggle = _RTCC_CC_CTRL_CMOA_TOGGLE,
  rtccCompMatchOutActionClear = _RTCC_CC_CTRL_CMOA_CLEAR,
  rtccCompMatchOutActionSet = _RTCC_CC_CTRL_CMOA_SET
}
 
enum  RTCC_DayCompareMode_TypeDef {
  rtccDayCompareModeMonth = _RTCC_CC_CTRL_DAYCC_MONTH,
  rtccDayCompareModeWeek = _RTCC_CC_CTRL_DAYCC_WEEK
}
 
enum  RTCC_InEdgeSel_TypeDef {
  rtccInEdgeRising = _RTCC_CC_CTRL_ICEDGE_RISING,
  rtccInEdgeFalling = _RTCC_CC_CTRL_ICEDGE_FALLING,
  rtccInEdgeBoth = _RTCC_CC_CTRL_ICEDGE_BOTH,
  rtccInEdgeNone = _RTCC_CC_CTRL_ICEDGE_NONE
}
 
enum  RTCC_PrescMode_TypeDef {
  rtccCntTickPresc = _RTCC_CTRL_CNTTICK_PRESC,
  rtccCntTickCCV0Match = _RTCC_CTRL_CNTTICK_CCV0MATCH
}
 
enum  RTCC_PRSSel_TypeDef {
  rtccPRSCh0 = _RTCC_CC_CTRL_PRSSEL_PRSCH0,
  rtccPRSCh1 = _RTCC_CC_CTRL_PRSSEL_PRSCH1,
  rtccPRSCh2 = _RTCC_CC_CTRL_PRSSEL_PRSCH2,
  rtccPRSCh3 = _RTCC_CC_CTRL_PRSSEL_PRSCH3,
  rtccPRSCh4 = _RTCC_CC_CTRL_PRSSEL_PRSCH4,
  rtccPRSCh5 = _RTCC_CC_CTRL_PRSSEL_PRSCH5,
  rtccPRSCh6 = _RTCC_CC_CTRL_PRSSEL_PRSCH6,
  rtccPRSCh7 = _RTCC_CC_CTRL_PRSSEL_PRSCH7,
  rtccPRSCh8 = _RTCC_CC_CTRL_PRSSEL_PRSCH8,
  rtccPRSCh9 = _RTCC_CC_CTRL_PRSSEL_PRSCH9,
  rtccPRSCh10 = _RTCC_CC_CTRL_PRSSEL_PRSCH10,
  rtccPRSCh11 = _RTCC_CC_CTRL_PRSSEL_PRSCH11
}
 

Functions

__STATIC_INLINE uint32_t RTCC_ChannelCCVGet (int ch)
 Get RTCC capture/compare register value (CCV) for selected channel.
 
__STATIC_INLINE void RTCC_ChannelCCVSet (int ch, uint32_t value)
 Set RTCC capture/compare register value (CCV) for selected channel.
 
__STATIC_INLINE uint32_t RTCC_ChannelDateGet (int ch)
 Get the calendar DATE register content for selected channel.
 
__STATIC_INLINE void RTCC_ChannelDateSet (int ch, uint32_t date)
 Set the calendar DATE register for selected channel.
 
void RTCC_ChannelInit (int ch, RTCC_CCChConf_TypeDef const *confPtr)
 Configure the selected capture/compare channel of the RTCC.
 
__STATIC_INLINE uint32_t RTCC_ChannelTimeGet (int ch)
 Get the calendar TIME register content for selected channel.
 
__STATIC_INLINE void RTCC_ChannelTimeSet (int ch, uint32_t time)
 Set the calendar TIME register for selected channel.
 
__STATIC_INLINE uint32_t RTCC_CombinedCounterGet (void)
 Get the combined CNT/PRECNT register content.
 
__STATIC_INLINE uint32_t RTCC_CounterGet (void)
 Get RTCC counter value.
 
__STATIC_INLINE void RTCC_CounterSet (uint32_t value)
 Set RTCC CNT counter.
 
__STATIC_INLINE uint32_t RTCC_DateGet (void)
 Get DATE register value.
 
__STATIC_INLINE void RTCC_DateSet (uint32_t date)
 Set RTCC DATE register.
 
__STATIC_INLINE void RTCC_EM4WakeupEnable (bool enable)
 Enable/disable EM4 wakeup capability.
 
void RTCC_Enable (bool enable)
 Enable/disable RTCC.
 
void RTCC_Init (const RTCC_Init_TypeDef *init)
 Initialize RTCC.
 
__STATIC_INLINE void RTCC_IntClear (uint32_t flags)
 Clear one or more pending RTCC interrupts.
 
__STATIC_INLINE void RTCC_IntDisable (uint32_t flags)
 Disable one or more RTCC interrupts.
 
__STATIC_INLINE void RTCC_IntEnable (uint32_t flags)
 Enable one or more RTCC interrupts.
 
__STATIC_INLINE uint32_t RTCC_IntGet (void)
 Get pending RTCC interrupt flags.
 
__STATIC_INLINE uint32_t RTCC_IntGetEnabled (void)
 Get enabled and pending RTCC interrupt flags.
 
__STATIC_INLINE void RTCC_IntSet (uint32_t flags)
 Set one or more pending RTCC interrupts from SW.
 
__STATIC_INLINE void RTCC_Lock (void)
 Lock RTCC registers.
 
__STATIC_INLINE uint32_t RTCC_PreCounterGet (void)
 Get RTCC pre-counter value.
 
__STATIC_INLINE void RTCC_PreCounterSet (uint32_t preCntVal)
 Set RTCC pre-counter value.
 
void RTCC_Reset (void)
 Restore RTCC to its reset state.
 
__STATIC_INLINE void RTCC_RetentionRamPowerDown (void)
 Power down the retention ram.
 
void RTCC_StatusClear (void)
 Clear STATUS register.
 
__STATIC_INLINE uint32_t RTCC_StatusGet (void)
 Get STATUS register value.
 
__STATIC_INLINE uint32_t RTCC_TimeGet (void)
 Get TIME register value.
 
__STATIC_INLINE void RTCC_TimeSet (uint32_t time)
 Set RTCC TIME register.
 
__STATIC_INLINE void RTCC_Unlock (void)
 Unlock RTCC registers.
 

Macro Definition Documentation

#define RTCC_CH_INIT_CAPTURE_DEFAULT
Value:
{ \
rtccCapComChModeCapture, /* Select input capture mode. */ \
rtccCompMatchOutActionPulse, /* Create pulse on capture. */ \
rtccPRSCh0, /* PRS channel 0. */ \
rtccInEdgeRising, /* Rising edge detection. */ \
rtccCompBaseCnt, /* Don't care. */ \
0, /* Don't care. */ \
rtccDayCompareModeMonth /* Don't care */ \
}

Default RTCC channel input capture init structure.

Definition at line 292 of file em_rtcc.h.

#define RTCC_CH_INIT_COMPARE_DEFAULT
Value:
{ \
rtccCapComChModeCompare, /* Select output compare mode. */ \
rtccCompMatchOutActionPulse, /* Create pulse on compare match.*/ \
rtccPRSCh0, /* PRS channel 0 (not used). */ \
rtccInEdgeNone, /* No edge detection. */ \
rtccCompBaseCnt, /* Counter comparison base. */ \
0, /* No compare mask bits set. */ \
rtccDayCompareModeMonth /* Don't care */ \
}

Default RTCC channel output compare init structure.

Definition at line 280 of file em_rtcc.h.

#define RTCC_CH_VALID (   ch)    ( (ch) < 3)

Validation of valid RTCC channel for assert statements.

Definition at line 304 of file em_rtcc.h.

Referenced by RTCC_ChannelCCVGet(), RTCC_ChannelCCVSet(), RTCC_ChannelDateGet(), RTCC_ChannelDateSet(), RTCC_ChannelInit(), RTCC_ChannelTimeGet(), and RTCC_ChannelTimeSet().

#define RTCC_INIT_DEFAULT
Value:
{ \
true, /* Start counting when init done. */ \
false, /* Disable RTCC during debug halt. */ \
false, /* Disable precounter wrap on ch. 0 CCV value. */ \
false, /* Disable counter wrap on ch. 1 CCV value. */ \
rtccCntPresc_32, /* 977 us per tick. */ \
rtccCntTickPresc, /* Counter increments according to prescaler value.*/ \
false, /* No RTCC oscillator failure detection. */ \
rtccCntModeNormal, /* Normal RTCC mode. */ \
false, /* No leap year correction. */ \
}

Default RTCC init structure.

Definition at line 265 of file em_rtcc.h.

Referenced by UDELAY_Calibrate().

Enumeration Type Documentation

Capture/Compare channel mode.

Enumerator
rtccCapComChModeOff 

Capture/Compare channel turned off.

rtccCapComChModeCapture 

Capture mode.

rtccCapComChModeCompare 

Compare mode.

Definition at line 116 of file em_rtcc.h.

Operational mode of the counter.

Enumerator
rtccCntModeNormal 

Normal counter mode. The counter is incremented by 1 for each tick.

rtccCntModeCalendar 

Calendar mode. Refer to the RTCC chapter of the Reference Manual for more details on the calendar mode.

Definition at line 76 of file em_rtcc.h.

Counter prescaler selection.

Enumerator
rtccCntPresc_1 

Divide clock by 1.

rtccCntPresc_2 

Divide clock by 2.

rtccCntPresc_4 

Divide clock by 4.

rtccCntPresc_8 

Divide clock by 8.

rtccCntPresc_16 

Divide clock by 16.

rtccCntPresc_32 

Divide clock by 32.

rtccCntPresc_64 

Divide clock by 64.

rtccCntPresc_128 

Divide clock by 128.

rtccCntPresc_256 

Divide clock by 256.

rtccCntPresc_512 

Divide clock by 512.

rtccCntPresc_1024 

Divide clock by 1024.

rtccCntPresc_2048 

Divide clock by 2048.

rtccCntPresc_4096 

Divide clock by 4096.

rtccCntPresc_8192 

Divide clock by 8192.

rtccCntPresc_16384 

Divide clock by 16384.

rtccCntPresc_32768 

Divide clock by 32768.

Definition at line 86 of file em_rtcc.h.

Capture/Compare channel compare mode.

Enumerator
rtccCompBaseCnt 

CCVx is compared with the CNT register.

rtccCompBasePreCnt 

CCVx is compared with a CNT[16:0] and PRECNT[14:0].

Definition at line 163 of file em_rtcc.h.

Compare match output action mode.

Enumerator
rtccCompMatchOutActionPulse 

Generate a pulse.

rtccCompMatchOutActionToggle 

Toggle output.

rtccCompMatchOutActionClear 

Clear output.

rtccCompMatchOutActionSet 

Set output.

Definition at line 123 of file em_rtcc.h.

Day compare mode.

Enumerator
rtccDayCompareModeMonth 

Day of month is selected for Capture/Compare.

rtccDayCompareModeWeek 

Day of week is selected for Capture/Compare.

Definition at line 172 of file em_rtcc.h.

Input edge select.

Enumerator
rtccInEdgeRising 

Rising edges detected.

rtccInEdgeFalling 

Falling edges detected.

rtccInEdgeBoth 

Both edges detected.

rtccInEdgeNone 

No edge detection, signal is left as is.

Definition at line 155 of file em_rtcc.h.

Prescaler mode of the RTCC counter.

Enumerator
rtccCntTickPresc 

CNT register ticks according to the prescaler value.

rtccCntTickCCV0Match 

CNT register ticks when PRECNT matches the 15 least significant bits of ch. 0 CCV register.

Definition at line 106 of file em_rtcc.h.

PRS input sources.

Enumerator
rtccPRSCh0 

PRS channel 0.

rtccPRSCh1 

PRS channel 1.

rtccPRSCh2 

PRS channel 2.

rtccPRSCh3 

PRS channel 3.

rtccPRSCh4 

PRS channel 4.

rtccPRSCh5 

PRS channel 5.

rtccPRSCh6 

PRS channel 6.

rtccPRSCh7 

PRS channel 7.

rtccPRSCh8 

PRS channel 8.

rtccPRSCh9 

PRS channel 9.

rtccPRSCh10 

PRS channel 10.

rtccPRSCh11 

PRS channel 11.

Definition at line 131 of file em_rtcc.h.

Function Documentation

__STATIC_INLINE uint32_t RTCC_ChannelCCVGet ( int  ch)

Get RTCC capture/compare register value (CCV) for selected channel.

Parameters
[in]chChannel selector.
Returns
Capture/compare register value.

Definition at line 320 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

__STATIC_INLINE void RTCC_ChannelCCVSet ( int  ch,
uint32_t  value 
)

Set RTCC capture/compare register value (CCV) for selected channel.

Parameters
[in]chChannel selector.
[in]valueCCV value.

Definition at line 336 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

__STATIC_INLINE uint32_t RTCC_ChannelDateGet ( int  ch)

Get the calendar DATE register content for selected channel.

Parameters
[in]chChannel selector.
Returns
DATE register value.

Definition at line 352 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

__STATIC_INLINE void RTCC_ChannelDateSet ( int  ch,
uint32_t  date 
)

Set the calendar DATE register for selected channel.

Parameters
[in]chChannel selector.
[in]dateDATE value.

Definition at line 368 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

void RTCC_ChannelInit ( int  ch,
RTCC_CCChConf_TypeDef const *  confPtr 
)

Configure the selected capture/compare channel of the RTCC.

Use this function to configure a RTCC channel. Select capture/compare mode, match output action, overflow output action and PRS input configuration. Refer to the configuration structure RTCC_CCChConf_TypeDef for more details.

Parameters
[in]chChannel selector.
[in]confPtrPointer to configuration structure.

Configure the selected capture/compare channel.

Definition at line 81 of file em_rtcc.c.

References _RTCC_CC_CTRL_CMOA_SHIFT, _RTCC_CC_CTRL_COMPBASE_SHIFT, _RTCC_CC_CTRL_COMPMASK_MASK, _RTCC_CC_CTRL_COMPMASK_SHIFT, _RTCC_CC_CTRL_DAYCC_SHIFT, _RTCC_CC_CTRL_ICEDGE_SHIFT, _RTCC_CC_CTRL_MODE_SHIFT, _RTCC_CC_CTRL_PRSSEL_SHIFT, RTCC_CCChConf_TypeDef::chMode, RTCC_CCChConf_TypeDef::compBase, RTCC_CCChConf_TypeDef::compMask, RTCC_CCChConf_TypeDef::compMatchOutAction, RTCC_CCChConf_TypeDef::dayCompMode, RTCC_CCChConf_TypeDef::inputEdgeSel, RTCC_CCChConf_TypeDef::prsSel, RTCC, and RTCC_CH_VALID.

Referenced by RTCDRV_Init().

__STATIC_INLINE uint32_t RTCC_ChannelTimeGet ( int  ch)

Get the calendar TIME register content for selected channel.

Parameters
[in]chChannel selector.
Returns
TIME register value.

Definition at line 386 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

__STATIC_INLINE void RTCC_ChannelTimeSet ( int  ch,
uint32_t  time 
)

Set the calendar TIME register for selected channel.

Parameters
[in]chChannel selector.
[in]timeTIME value.

Definition at line 402 of file em_rtcc.h.

References RTCC, and RTCC_CH_VALID.

__STATIC_INLINE uint32_t RTCC_CombinedCounterGet ( void  )

Get the combined CNT/PRECNT register content.

Returns
CNT/PRECNT register value.

Definition at line 415 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE uint32_t RTCC_CounterGet ( void  )

Get RTCC counter value.

Returns
Current RTCC counter value.

Definition at line 427 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_CounterSet ( uint32_t  value)

Set RTCC CNT counter.

Parameters
[in]valueCNT value.

Definition at line 439 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE uint32_t RTCC_DateGet ( void  )

Get DATE register value.

Returns
Current DATE register value.

Definition at line 451 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_DateSet ( uint32_t  date)

Set RTCC DATE register.

Parameters
[in]dateDATE value.

Definition at line 463 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_EM4WakeupEnable ( bool  enable)

Enable/disable EM4 wakeup capability.

Parameters
[in]enableTrue to enable EM4 wakeup, false to disable.

Definition at line 475 of file em_rtcc.h.

References RTCC, and RTCC_EM4WUEN_EM4WU.

void RTCC_Enable ( bool  enable)

Enable/disable RTCC.

Parameters
[in]enableTrue to enable RTCC, false to disable.

Definition at line 105 of file em_rtcc.c.

References _RTCC_CTRL_ENABLE_SHIFT, BUS_RegBitWrite(), and RTCC.

Referenced by RTCDRV_DeInit(), and UDELAY_Calibrate().

void RTCC_Init ( const RTCC_Init_TypeDef init)

Initialize RTCC.

Note that the compare values must be set separately with RTCC_CompareSet(). That should probably be done prior to the use of this function if configuring the RTCC to start when initialization is completed.

Parameters
[in]initPointer to RTCC initialization structure.

Definition at line 123 of file em_rtcc.c.

References _RTCC_CTRL_CCV1TOP_SHIFT, _RTCC_CTRL_CNTMODE_SHIFT, _RTCC_CTRL_CNTPRESC_SHIFT, _RTCC_CTRL_CNTTICK_SHIFT, _RTCC_CTRL_DEBUGRUN_SHIFT, _RTCC_CTRL_ENABLE_SHIFT, _RTCC_CTRL_LYEARCORRDIS_SHIFT, _RTCC_CTRL_OSCFDETEN_SHIFT, _RTCC_CTRL_PRECCV0TOP_SHIFT, RTCC_Init_TypeDef::cntMode, RTCC_Init_TypeDef::cntWrapOnCCV1, RTCC_Init_TypeDef::debugRun, RTCC_Init_TypeDef::disLeapYearCorr, RTCC_Init_TypeDef::enable, RTCC_Init_TypeDef::enaOSCFailDetect, RTCC_Init_TypeDef::precntWrapOnCCV0, RTCC_Init_TypeDef::presc, RTCC_Init_TypeDef::prescMode, and RTCC.

Referenced by RTCDRV_Init(), and UDELAY_Calibrate().

__STATIC_INLINE void RTCC_IntClear ( uint32_t  flags)

Clear one or more pending RTCC interrupts.

Parameters
[in]flagsRTCC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources.

Definition at line 496 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_IntDisable ( uint32_t  flags)

Disable one or more RTCC interrupts.

Parameters
[in]flagsRTCC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt.

Definition at line 509 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_IntEnable ( uint32_t  flags)

Enable one or more RTCC interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using RTCC_IntClear() prior to enabling if such a pending interrupt should be ignored.
Parameters
[in]flagsRTCC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt.

Definition at line 527 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE uint32_t RTCC_IntGet ( void  )

Get pending RTCC interrupt flags.

Note
The event bits are not cleared by the use of this function.
Returns
Pending RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.

Definition at line 543 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE uint32_t RTCC_IntGetEnabled ( void  )

Get enabled and pending RTCC interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Returns
Pending and enabled RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.

Definition at line 559 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_IntSet ( uint32_t  flags)

Set one or more pending RTCC interrupts from SW.

Parameters
[in]flagsRTCC interrupt sources to set to pending. Use a set of interrupt flags (RTCC_IFS_nnn).

Definition at line 577 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_Lock ( void  )

Lock RTCC registers.

Note
When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers can not be written to.

Definition at line 591 of file em_rtcc.h.

References CMU, CMU_LOCK_LOCKKEY_LOCK, CMU_LOCK_LOCKKEY_LOCKED, CMU_LOCK_LOCKKEY_UNLOCK, RTCC, and RTCC_LOCK_LOCKKEY_LOCK.

__STATIC_INLINE uint32_t RTCC_PreCounterGet ( void  )

Get RTCC pre-counter value.

Returns
Current RTCC pre-counter value.

Definition at line 620 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_PreCounterSet ( uint32_t  preCntVal)

Set RTCC pre-counter value.

Parameters
[in]preCntValRTCC pre-counter value to be set.

Definition at line 632 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_RetentionRamPowerDown ( void  )

Power down the retention ram.

Note
Once retention ram is powered down, it cannot be powered up again.

Definition at line 646 of file em_rtcc.h.

References RTCC, and RTCC_POWERDOWN_RAM.

__STATIC_INLINE uint32_t RTCC_StatusGet ( void  )

Get STATUS register value.

Returns
Current STATUS register value.

Definition at line 664 of file em_rtcc.h.

References RTCC, and RTCC_SYNCBUSY_CMD.

__STATIC_INLINE uint32_t RTCC_TimeGet ( void  )

Get TIME register value.

Returns
Current TIME register value.

Definition at line 679 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_TimeSet ( uint32_t  time)

Set RTCC TIME register.

Parameters
[in]timeTIME value.

Definition at line 691 of file em_rtcc.h.

References RTCC.

__STATIC_INLINE void RTCC_Unlock ( void  )

Unlock RTCC registers.

Note
When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers can not be written to.

Definition at line 705 of file em_rtcc.h.

References CMU, CMU_LOCK_LOCKKEY_LOCK, CMU_LOCK_LOCKKEY_LOCKED, CMU_LOCK_LOCKKEY_UNLOCK, RTCC, and RTCC_LOCK_LOCKKEY_UNLOCK.

Referenced by RTCC_Reset().