CSEN_TypeDef Struct ReferenceDevices > CSEN

CSEN Register Declaration

Definition at line 49 of file efm32pg12b_csen.h .

#include < efm32pg12b_csen.h >

Data Fields

__IOM uint32_t ANACTRL
__IM uint32_t APORTCONFLICT
__IM uint32_t APORTREQ
__IOM uint32_t CMD
__IOM uint32_t CMPTHR
__IOM uint32_t CTRL
__IOM uint32_t DATA
__IOM uint32_t DMBASELINE
__IOM uint32_t DMCFG
__IOM uint32_t EMA
__IOM uint32_t EMACTRL
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t PRSSEL
uint32_t RESERVED0 [2]
__IOM uint32_t SCANINPUTSEL0
__IOM uint32_t SCANINPUTSEL1
__IOM uint32_t SCANMASK0
__IOM uint32_t SCANMASK1
__IOM uint32_t SINGLECTRL
__IM uint32_t STATUS
__IOM uint32_t TIMCTRL

Field Documentation

__IOM uint32_t CSEN_TypeDef::ANACTRL

Analog Control

Definition at line 68 of file efm32pg12b_csen.h .

Referenced by CSEN_InitMode() , and CSEN_Reset() .

__IM uint32_t CSEN_TypeDef::APORTCONFLICT

APORT Request Conflict

Definition at line 61 of file efm32pg12b_csen.h .

__IM uint32_t CSEN_TypeDef::APORTREQ

APORT Request Status

Definition at line 60 of file efm32pg12b_csen.h .

__IOM uint32_t CSEN_TypeDef::CMD

Command

Definition at line 52 of file efm32pg12b_csen.h .

Referenced by CSEN_Start() .

__IOM uint32_t CSEN_TypeDef::CMPTHR

Comparator Threshold

Definition at line 62 of file efm32pg12b_csen.h .

Referenced by CSEN_InitMode() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::CTRL

Control

Definition at line 50 of file efm32pg12b_csen.h .

Referenced by CSEN_Disable() , CSEN_Enable() , CSEN_Init() , CSEN_InitMode() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::DATA

Output Data

Definition at line 55 of file efm32pg12b_csen.h .

Referenced by CSEN_DataGet() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::DMBASELINE

Delta Modulation Baseline

Definition at line 66 of file efm32pg12b_csen.h .

Referenced by CSEN_DMBaselineSet() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::DMCFG

Delta Modulation Configuration

Definition at line 67 of file efm32pg12b_csen.h .

Referenced by CSEN_InitMode() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::EMA

Exponential Moving Average

Definition at line 63 of file efm32pg12b_csen.h .

Referenced by CSEN_EMAGet() , CSEN_EMASet() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::EMACTRL

Exponential Moving Average Control

Definition at line 64 of file efm32pg12b_csen.h .

Referenced by CSEN_InitMode() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::IEN

Interrupt Enable

Definition at line 74 of file efm32pg12b_csen.h .

Referenced by CSEN_IntDisable() , CSEN_IntEnable() , CSEN_IntGetEnabled() , and CSEN_Reset() .

__IM uint32_t CSEN_TypeDef::IF

Interrupt Flag

Definition at line 71 of file efm32pg12b_csen.h .

Referenced by CSEN_IntGet() , and CSEN_IntGetEnabled() .

__IOM uint32_t CSEN_TypeDef::IFC

Interrupt Flag Clear

Definition at line 73 of file efm32pg12b_csen.h .

Referenced by CSEN_IntClear() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::IFS

Interrupt Flag Set

Definition at line 72 of file efm32pg12b_csen.h .

Referenced by CSEN_IntSet() .

__IOM uint32_t CSEN_TypeDef::PRSSEL

PRS Select

Definition at line 54 of file efm32pg12b_csen.h .

Referenced by CSEN_Init() , and CSEN_Reset() .

uint32_t CSEN_TypeDef::RESERVED0[2]

Reserved for future use

Definition at line 70 of file efm32pg12b_csen.h .

__IOM uint32_t CSEN_TypeDef::SCANINPUTSEL0

Scan Input Selection 0

Definition at line 57 of file efm32pg12b_csen.h .

Referenced by CSEN_Init() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::SCANINPUTSEL1

Scan Input Selection 1

Definition at line 59 of file efm32pg12b_csen.h .

Referenced by CSEN_Init() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::SCANMASK0

Scan Channel Mask 0

Definition at line 56 of file efm32pg12b_csen.h .

Referenced by CSEN_InitMode() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::SCANMASK1

Scan Channel Mask 1

Definition at line 58 of file efm32pg12b_csen.h .

Referenced by CSEN_InitMode() , and CSEN_Reset() .

__IOM uint32_t CSEN_TypeDef::SINGLECTRL

Single Conversion Control

Definition at line 65 of file efm32pg12b_csen.h .

Referenced by CSEN_InitMode() , and CSEN_Reset() .

__IM uint32_t CSEN_TypeDef::STATUS

Status

Definition at line 53 of file efm32pg12b_csen.h .

Referenced by CSEN_IsBusy() .

__IOM uint32_t CSEN_TypeDef::TIMCTRL

Timing Control

Definition at line 51 of file efm32pg12b_csen.h .

Referenced by CSEN_Init() , and CSEN_Reset() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG12B/Include/ efm32pg12b_csen.h