WDOG_TypeDef Struct ReferenceDevices > WDOG

WDOG Register Declaration

Definition at line 49 of file efm32pg12b_wdog.h .

#include < efm32pg12b_wdog.h >

Data Fields

__IOM uint32_t CMD
__IOM uint32_t CTRL
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
WDOG_PCH_TypeDef PCH [2]
uint32_t RESERVED0 [2]
__IM uint32_t SYNCBUSY

Field Documentation

__IOM uint32_t WDOG_TypeDef::CMD

Command Register

Definition at line 51 of file efm32pg12b_wdog.h .

Referenced by WDOGn_Feed() .

__IOM uint32_t WDOG_TypeDef::CTRL

Control Register

Definition at line 50 of file efm32pg12b_wdog.h .

Referenced by WDOGn_Enable() , WDOGn_Feed() , WDOGn_Init() , and WDOGn_Lock() .

__IOM uint32_t WDOG_TypeDef::IEN

Interrupt Enable Register

Definition at line 61 of file efm32pg12b_wdog.h .

Referenced by WDOGn_IntDisable() , WDOGn_IntEnable() , and WDOGn_IntGetEnabled() .

__IM uint32_t WDOG_TypeDef::IF

Watchdog Interrupt Flags

Definition at line 58 of file efm32pg12b_wdog.h .

Referenced by WDOGn_IntGet() , and WDOGn_IntGetEnabled() .

__IOM uint32_t WDOG_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 60 of file efm32pg12b_wdog.h .

Referenced by WDOGn_IntClear() .

__IOM uint32_t WDOG_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 59 of file efm32pg12b_wdog.h .

Referenced by WDOGn_IntSet() .

WDOG_PCH_TypeDef WDOG_TypeDef::PCH[2]

PCH

Definition at line 55 of file efm32pg12b_wdog.h .

uint32_t WDOG_TypeDef::RESERVED0[2]

Reserved for future use

Definition at line 57 of file efm32pg12b_wdog.h .

__IM uint32_t WDOG_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 53 of file efm32pg12b_wdog.h .

Referenced by WDOGn_Enable() , WDOGn_Feed() , WDOGn_Init() , and WDOGn_Lock() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG12B/Include/ efm32pg12b_wdog.h