LESENSE_CH_TypeDef Struct ReferenceDevicesDevices > | LESENSE
LESENSE_CH LESENSE CH Register
.
Definition at line 47
of file efm32pg12b_lesense_ch.h
.
#include <
efm32pg12b_lesense_ch.h
>
Data Fields | |
__IOM uint32_t | EVAL |
__IOM uint32_t | INTERACT |
uint32_t | RESERVED0 [1] |
__IOM uint32_t | TIMING |
Field Documentation
__IOM uint32_t LESENSE_CH_TypeDef::EVAL |
Scan Configuration
Definition at line 50
of file efm32pg12b_lesense_ch.h
.
Referenced by LESENSE_ChannelSlidingWindow(), and LESENSE_ChannelStepDetection().
__IOM uint32_t LESENSE_CH_TypeDef::INTERACT |
Scan Configuration
Definition at line 49
of file efm32pg12b_lesense_ch.h
.
uint32_t LESENSE_CH_TypeDef::RESERVED0[1] |
Reserved future
Definition at line 51
of file efm32pg12b_lesense_ch.h
.
__IOM uint32_t LESENSE_CH_TypeDef::TIMING |
Scan Configuration
Definition at line 48
of file efm32pg12b_lesense_ch.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG12B/Include/
efm32pg12b_lesense_ch.h