ADC_InitSingle_TypeDef Struct ReferenceEMLIB > ADC
Single conversion init structure.
Definition at line 962
of file em_adc.h
.
#include <
em_adc.h
>
Data Fields | |
ADC_AcqTime_TypeDef | acqTime |
bool | diff |
bool | fifoOverwrite |
bool | leftAdjust |
ADC_NegSel_TypeDef | negSel |
ADC_PosSel_TypeDef | posSel |
bool | prsEnable |
ADC_PRSSEL_TypeDef | prsSel |
ADC_Ref_TypeDef | reference |
bool | rep |
ADC_Res_TypeDef | resolution |
bool | singleDmaEm2Wu |
Field Documentation
ADC_AcqTime_TypeDef ADC_InitSingle_TypeDef::acqTime |
Acquisition time (in ADC clock cycles).
Definition at line 970
of file em_adc.h
.
Referenced by ADC0_IRQHandler(), ADC_InitSingle(), and adcInit().
bool ADC_InitSingle_TypeDef::diff |
Select if single ended or differential input.
Definition at line 1001
of file em_adc.h
.
Referenced by ADC_InitSingle().
bool ADC_InitSingle_TypeDef::fifoOverwrite |
When true, the FIFO overwrites old data when full. If false, then the FIFO discards new data. The SCANOF IRQ is triggered in both cases.
Definition at line 1020
of file em_adc.h
.
Referenced by ADC_InitSingle().
bool ADC_InitSingle_TypeDef::leftAdjust |
Select if left adjustment should be done.
Definition at line 1007
of file em_adc.h
.
Referenced by ADC_InitSingle().
ADC_NegSel_TypeDef ADC_InitSingle_TypeDef::negSel |
Select negative input for single channel conversion mode. Negative input is grounded for single ended (non-differential) converison.
Definition at line 997
of file em_adc.h
.
Referenced by ADC_InitSingle(), and adcInit().
ADC_PosSel_TypeDef ADC_InitSingle_TypeDef::posSel |
Select positive input for for single channel conversion mode.
Definition at line 991
of file em_adc.h
.
Referenced by ADC_InitSingle(), and adcInit().
bool ADC_InitSingle_TypeDef::prsEnable |
Peripheral reflex system trigger enable.
Definition at line 1004
of file em_adc.h
.
Referenced by ADC_InitSingle(), and adcInit().
ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if prsEnable
is enabled.
Definition at line 967
of file em_adc.h
.
Referenced by ADC_InitSingle(), and adcInit().
ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference |
Sample reference selection. Notice that for external references, the ADC calibration register must be set explicitly.
Definition at line 976
of file em_adc.h
.
Referenced by ADC0_IRQHandler(), ADC_InitSingle(), adcInit(), and TOUCH_Init().
bool ADC_InitSingle_TypeDef::rep |
Select if continuous conversion until explicit stop.
Definition at line 1010
of file em_adc.h
.
Referenced by ADC_InitSingle().
ADC_Res_TypeDef ADC_InitSingle_TypeDef::resolution |
Sample resolution.
Definition at line 979
of file em_adc.h
.
Referenced by ADC0_IRQHandler(), ADC_InitSingle(), and TOUCH_Init().
bool ADC_InitSingle_TypeDef::singleDmaEm2Wu |
When true, DMA is available in EM2 for single conversion
Definition at line 1014
of file em_adc.h
.
Referenced by ADC_InitSingle().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_adc.h