RTCC_CCChConf_TypeDef Struct ReferenceEMLIB > RTCC
RTCC capture/compare channel configuration structure.
Definition at line 221
of file em_rtcc.h
.
#include <
em_rtcc.h
>
Field Documentation
RTCC_CapComChMode_TypeDef RTCC_CCChConf_TypeDef::chMode |
Select the mode of the Capture/Compare channel.
Definition at line 223
of file em_rtcc.h
.
Referenced by RTCC_ChannelInit().
RTCC_CompBase_TypeDef RTCC_CCChConf_TypeDef::compBase |
Comparison base of the channel in compare mode.
Definition at line 235
of file em_rtcc.h
.
Referenced by RTCC_ChannelInit().
uint8_t RTCC_CCChConf_TypeDef::compMask |
The COMPMASK (5 bit) most significant bits of the compare value will not be subject to comparison.
Definition at line 239
of file em_rtcc.h
.
Referenced by RTCC_ChannelInit().
RTCC_CompMatchOutAction_TypeDef RTCC_CCChConf_TypeDef::compMatchOutAction |
Compare mode channel match output action.
Definition at line 226
of file em_rtcc.h
.
Referenced by RTCC_ChannelInit().
RTCC_DayCompareMode_TypeDef RTCC_CCChConf_TypeDef::dayCompMode |
RTCC_InEdgeSel_TypeDef RTCC_CCChConf_TypeDef::inputEdgeSel |
Capture mode channel input edge selection.
Definition at line 232
of file em_rtcc.h
.
Referenced by RTCC_ChannelInit().
RTCC_PRSSel_TypeDef RTCC_CCChConf_TypeDef::prsSel |
Capture mode channel PRS input channel selection.
Definition at line 229
of file em_rtcc.h
.
Referenced by RTCC_ChannelInit().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_rtcc.h