RMU_TypeDef Struct ReferenceDevices > RMU
RMU Register Declaration
Definition at line 49
of file efm32pg12b_rmu.h
.
#include <
efm32pg12b_rmu.h
>
Data Fields | |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IOM uint32_t | LOCK |
__IOM uint32_t | RST |
__IM uint32_t | RSTCAUSE |
Field Documentation
__IOM uint32_t RMU_TypeDef::CMD |
Command Register
Definition at line 52
of file efm32pg12b_rmu.h
.
__IOM uint32_t RMU_TypeDef::CTRL |
Control Register
Definition at line 50
of file efm32pg12b_rmu.h
.
__IOM uint32_t RMU_TypeDef::LOCK |
Configuration Lock Register
Definition at line 54
of file efm32pg12b_rmu.h
.
__IOM uint32_t RMU_TypeDef::RST |
Reset Control Register
Definition at line 53
of file efm32pg12b_rmu.h
.
__IM uint32_t RMU_TypeDef::RSTCAUSE |
Reset Cause Register
Definition at line 51
of file efm32pg12b_rmu.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG12B/Include/
efm32pg12b_rmu.h