GPIO_P_TypeDef Struct ReferenceDevicesDevices > | GPIO
GPIO_P GPIO P Register
.
Definition at line 47
of file efm32pg12b_gpio_p.h
.
#include <
efm32pg12b_gpio_p.h
>
Data Fields | |
__IOM uint32_t | CTRL |
__IM uint32_t | DIN |
__IOM uint32_t | DOUT |
__IOM uint32_t | DOUTTGL |
__IOM uint32_t | MODEH |
__IOM uint32_t | MODEL |
__IOM uint32_t | OVTDIS |
__IOM uint32_t | PINLOCKN |
uint32_t | RESERVED0 [2] |
uint32_t | RESERVED1 [1] |
uint32_t | RESERVED2 [1] |
Field Documentation
__IOM uint32_t GPIO_P_TypeDef::CTRL |
Port Control Register
Definition at line 48
of file efm32pg12b_gpio_p.h
.
__IM uint32_t GPIO_P_TypeDef::DIN |
Port Data in Register
Definition at line 54
of file efm32pg12b_gpio_p.h
.
__IOM uint32_t GPIO_P_TypeDef::DOUT |
Port Data Out Register
Definition at line 51
of file efm32pg12b_gpio_p.h
.
__IOM uint32_t GPIO_P_TypeDef::DOUTTGL |
Port Data Out Toggle Register
Definition at line 53
of file efm32pg12b_gpio_p.h
.
__IOM uint32_t GPIO_P_TypeDef::MODEH |
Port Pin Mode High Register
Definition at line 50
of file efm32pg12b_gpio_p.h
.
__IOM uint32_t GPIO_P_TypeDef::MODEL |
Port Pin Mode Low Register
Definition at line 49
of file efm32pg12b_gpio_p.h
.
__IOM uint32_t GPIO_P_TypeDef::OVTDIS |
Over Voltage Disable for All Modes
Definition at line 57
of file efm32pg12b_gpio_p.h
.
__IOM uint32_t GPIO_P_TypeDef::PINLOCKN |
Port Unlocked Pins Register
Definition at line 55
of file efm32pg12b_gpio_p.h
.
uint32_t GPIO_P_TypeDef::RESERVED0[2] |
Reserved for future use
Definition at line 52
of file efm32pg12b_gpio_p.h
.
uint32_t GPIO_P_TypeDef::RESERVED1[1] |
Reserved for future use
Definition at line 56
of file efm32pg12b_gpio_p.h
.
uint32_t GPIO_P_TypeDef::RESERVED2[1] |
Reserved future
Definition at line 58
of file efm32pg12b_gpio_p.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG12B/Include/
efm32pg12b_gpio_p.h