EM_TypeDef Struct Reference

Defines segment COM and BIT fields for Energy Modes on display.

Definition at line 82 of file segmentlcd.c.

Data Fields

uint8_t bit [5]
 
uint8_t com [5]
 

Field Documentation

uint8_t EM_TypeDef::bit[5]

LCD bit number

Definition at line 84 of file segmentlcd.c.

Referenced by SegmentLCD_EnergyMode().

uint8_t EM_TypeDef::com[5]

LCD COM line (for multiplexing)

Definition at line 83 of file segmentlcd.c.

Referenced by SegmentLCD_EnergyMode().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/hardware/kit/common/drivers/segmentlcd.c