gpiointerrupt.h File Reference

GPIOINT API definition.

Version
5.5.0

License

(C) Copyright 2014 Silicon Labs, www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file gpiointerrupt.h.

#include "em_device.h"

Typedefs

typedef void(* GPIOINT_IrqCallbackPtr_t) (uint8_t pin)
 GPIO interrupt callback function pointer.
 

Functions

void GPIOINT_CallbackRegister (uint8_t pin, GPIOINT_IrqCallbackPtr_t callbackPtr)
 Registers user callback for given pin number.
 
static __INLINE void GPIOINT_CallbackUnRegister (uint8_t pin)
 Unregisters user callback for given pin number.
 
void GPIOINT_Init (void)
 Initialization of GPIOINT module.