caplesense.c File Reference
Capacitive sense driver.
- Version
- 5.5.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        caplesense.c
       
       .
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        caplesense.h
       
       "
      
      
       #include "
       
        em_emu.h
       
       "
      
      
       #include "
       
        em_acmp.h
       
       "
      
      
       #include "
       
        em_assert.h
       
       "
      
      
       #include "
       
        em_cmu.h
       
       "
      
      
       #include "
       
        em_gpio.h
       
       "
      
      
       #include "
       
        em_core.h
       
       "
      
      
       #include "
       
        em_lesense.h
       
       "
      
      
       #include "caplesenseconfig.h"
      
      
| Functions | |
| uint32_t | CAPLESENSE_getNormalizedVal (uint8_t channel) | 
| Get the current normalized channelValue for a channel. | |
| uint8_t | CAPLESENSE_getSegmentChannel (uint8_t capSegment) | 
| Get the channelValue for a sensor segment. | |
| int32_t | CAPLESENSE_getSliderPosition (void) | 
| Get the position of the slider. | |
| uint32_t | CAPLESENSE_getVal (uint8_t channel) | 
| Get the current channelValue for a channel. | |
| void | CAPLESENSE_Init (bool sleep) | 
| Initializes the capacative sense system without LESENSE. | |
| void | CAPLESENSE_setupACMP (void) | 
| Setup the ACMP. | |
| void | CAPLESENSE_setupCallbacks (void(*scanCb)(void), void(*chCb)(void)) | 
| LESENSE callback setup. | |
| void | CAPLESENSE_setupCMU (void) | 
| Setup the CMU. | |
| void | CAPLESENSE_setupGPIO (void) | 
| Setup the GPIO. | |
| void | CAPLESENSE_setupLESENSE (bool sleep) | 
| Setup the LESENSE for capavitive sensing. | |
| void | CAPLESENSE_Sleep (void) | 
| Send the capacative sense system to sleep mode. | |
| void | LESENSE_IRQHandler (void) | 
| LESENSE interrupt handler. | |
| Variables | |
| static volatile uint32_t | channelMaxValues [LESENSE_CHANNELS] | 
| This stores the maximum values seen by a channel. | |
| static const bool | channelsInUse [LESENSE_CHANNELS] = LESENSE_CAPSENSE_CH_IN_USE | 
| A bit vector which represents the channels to iterate through. | |
| static volatile uint32_t | channelValues [LESENSE_CHANNELS] | 
| This vector stores the latest read values from LESENSE. | |
| static volatile uint8_t | currentChannel | 
| static void(* | lesenseChCb )(void) | 
| static void(* | lesenseScanCb )(void) | 
Function Documentation
| void CAPLESENSE_setupCMU | ( | void | 
            | ) | 
Setup the CMU.
Prototypes
        Definition at line
        
         84
        
        of file
        
         caplesense.c
        
        .
       
References CMU_ClockDivSet() , CMU_ClockEnable() , CMU_ClockSelectSet() , cmuClkDiv_1 , cmuClock_ACMP0 , cmuClock_ACMP1 , cmuClock_GPIO , cmuClock_HF , cmuClock_HFPER , cmuClock_LESENSE , cmuClock_LFA , cmuClock_LFB , cmuSelect_Disabled , cmuSelect_HFRCO , cmuSelect_LFRCO , and SystemCoreClockUpdate() .
Referenced by CAPLESENSE_Init() .
Variable Documentation
| 
 | static | 
This stores the maximum values seen by a channel.
- Parameters
- 
         LESENSE_CHANNELSVector of channels. 
        Definition at line
        
         49
        
        of file
        
         caplesense.c
        
        .
       
Referenced by CAPLESENSE_getNormalizedVal() , CAPLESENSE_getSliderPosition() , CAPSENSE_getNormalizedVal() , CAPSENSE_getPressed() , CAPSENSE_getSliderPosition() , LESENSE_IRQHandler() , and TIMER0_IRQHandler() .
| 
 | static | 
A bit vector which represents the channels to iterate through.
- Parameters
- 
         LESENSE_CHANNELSVector of channels. 
        Definition at line
        
         61
        
        of file
        
         caplesense.c
        
        .
       
Referenced by CAPLESENSE_setupLESENSE() , CAPSENSE_Sense() , and LESENSE_IRQHandler() .
| 
 | static | 
This vector stores the latest read values from LESENSE.
- Parameters
- 
         LESENSE_CHANNELSVector of channels. 
        Definition at line
        
         37
        
        of file
        
         caplesense.c
        
        .
       
Referenced by CAPLESENSE_getNormalizedVal() , CAPLESENSE_getSliderPosition() , CAPLESENSE_getVal() , CAPSENSE_getNormalizedVal() , CAPSENSE_getPressed() , CAPSENSE_getSliderPosition() , CAPSENSE_getVal() , LESENSE_IRQHandler() , and TIMER0_IRQHandler() .
| 
 | static | 
The current channel we are sensing
        Definition at line
        
         79
        
        of file
        
         caplesense.c
        
        .
       
Referenced by CAPSENSE_Sense() , LESENSE_IRQHandler() , and TIMER0_IRQHandler() .
| 
 | static | 
Callback function for LESENSE interrupts.
        Definition at line
        
         76
        
        of file
        
         caplesense.c
        
        .
       
Referenced by CAPLESENSE_setupCallbacks() , and LESENSE_IRQHandler() .
| 
 | static | 
Local variablesCallback function for LESENSE interrupts.
        Definition at line
        
         74
        
        of file
        
         caplesense.c
        
        .
       
Referenced by CAPLESENSE_setupCallbacks() , and LESENSE_IRQHandler() .