operand_t Struct Reference
The fx20_divide and fx20_multiply uses this structure to pass values into it.
Definition at line 1020
of file si114x_functions.c
.
Data Fields | |
uint32_t | op1 |
uint32_t | op2 |
Field Documentation
uint32_t operand_t::op1 |
uint32_t operand_t::op2 |
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/hardware/kit/common/drivers/
si114x_functions.c