em_usbxpress_callback.c File Reference
Contains call-back functions from the EFM32 USB Library.
- Version
- 5.6.0
License
Copyright 2016 Silicon Laboratories, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
em_usbxpress_callback.c
.
#include <stddef.h>
#include "
em_usbxpress_internal.h
"
#include "
em_usbxpress_descriptors.h
"
#include "
em_usbxpress.h
"
Functions |
|
| static uint8_t usbxpressPartNumber | SL_ATTRIBUTE_ALIGN (4) |
|
USBXpress Part Number.
|
|
| void | USBX_DeviceStateChangeCb ( USBD_State_TypeDef oldState, USBD_State_TypeDef newState) |
|
USB device state change call-back.
|
|
| int | USBX_inXferCompleteCb ( USB_Status_TypeDef status, uint16_t xferred, uint16_t remaining) |
|
USBXpress IN Endpoint Transfer Complete Callback.
|
|
| int | USBX_outXferCompleteCb ( USB_Status_TypeDef status, uint16_t xferred, uint16_t remaining) |
|
USBXpress OUT Endpoint Transfer Complete Callback.
|
|
| void | USBX_ResetCb (void) |
|
USB Reset call-back.
|
|
| int | USBX_SetupCmdCb (const USB_Setup_TypeDef *setup) |
|
USB setup command call-back.
|
|
Variables |
|
| uint8_t | USBXCORE_overflowBuffer [] |
| bool | USBXCORE_rxOverflowPacketAvailable |
|
Boolean indicating if data was received while expecting a ZLP.
|
|
| uint32_t | USBXCORE_rxOverflowPacketSize |
|
Size of Rx Overflow Packet.
|
|
| bool | USBXCORE_zlpActive |
|
Boolean indicating whether a ZLP read is active.
|
|
Function Documentation
|
static |
USBXpress Part Number.
USBXpress Library Version.
| void USBX_DeviceStateChangeCb | ( | USBD_State_TypeDef |
oldState,
|
| USBD_State_TypeDef |
newState
|
||
| ) |
USB device state change call-back.
Set new state and jump to user API call-back.
Definition at line
71
of file
em_usbxpress_callback.c
.
References
APIEA_GIE
,
USBD_STATE_CONFIGURED
,
USBD_STATE_SUSPENDED
,
USBX_DEV_CONFIGURED
,
USBX_DEV_SUSPEND
,
USBX_jumpCallback()
,
USBXCORE_apiEa
,
USBXCORE_apiIntValue
, and
USBXCORE_resetState()
.
Referenced by USBX_init() .
| int USBX_inXferCompleteCb | ( | USB_Status_TypeDef |
status,
|
| uint16_t |
xferred,
|
||
| uint16_t |
remaining
|
||
| ) |
USBXpress IN Endpoint Transfer Complete Callback.
Gets the number of IN bytes transferred and passes them to the user API call-back.
Definition at line
242
of file
em_usbxpress_callback.c
.
References
APIEA_GIE
,
USB_FS_BULK_EP_MAXSIZE
,
USB_STATUS_OK
,
USBD_Write()
,
USBX_jumpCallback()
,
USBX_TX_COMPLETE
,
USBXCORE_apiEa
,
USBXCORE_apiIntValue
,
USBXCORE_byteCountInPtr
, and
USBXCORE_writeSize
.
Referenced by USBX_blockWrite() .
| int USBX_outXferCompleteCb | ( | USB_Status_TypeDef |
status,
|
| uint16_t |
xferred,
|
||
| uint16_t |
remaining
|
||
| ) |
USBXpress OUT Endpoint Transfer Complete Callback.
Gets the number of OUT bytes transferred and passes them to the user API call-back.
Definition at line
282
of file
em_usbxpress_callback.c
.
References
APIEA_GIE
,
USB_STATUS_OK
,
USBD_Read()
,
USBX_jumpCallback()
,
USBX_RX_COMPLETE
,
USBX_RX_OVERRUN
,
USBXCORE_apiEa
,
USBXCORE_apiIntValue
,
USBXCORE_byteCountOutPtr
, and
USBXCORE_readSize
.
Referenced by USBX_blockRead() .
| void USBX_ResetCb | ( | void |
|
) |
USB Reset call-back.
Jump to user API RESET call-back.
Definition at line
54
of file
em_usbxpress_callback.c
.
References
APIEA_GIE
,
USBX_jumpCallback()
,
USBX_RESET
,
USBXCORE_apiEa
,
USBXCORE_apiIntValue
, and
USBXCORE_resetState()
.
Referenced by USBX_init() .
| int USBX_SetupCmdCb | ( | const USB_Setup_TypeDef * |
setup
|
) |
USB setup command call-back.
If the setup command is a vendor request, pass to the USB command request parsing routine and acknowledge. Otherwise ignore the request.
Definition at line
101
of file
em_usbxpress_callback.c
.
References
APIEA_GIE
,
APIEA_GIE_TEMP
,
USB_Setup_TypeDef::bmRequestType
,
USB_Setup_TypeDef::bRequest
,
EXT_COMP_DESC_SIZE
,
EXT_COMP_VENDOR_CODE
,
FEATURE_EXTENDED_COMPATIBILITY_ID
,
FEATURE_EXTENDED_PROPERTIES_ID
,
GET_DESCRIPTOR
,
PROPERTIES_DESCRIPTOR_SIZE
,
SI_CP210X_GET_PART_NUMBER
,
SI_CP210X_REQUEST
,
SI_USBXPRESS_CLEAR_TO_SEND
,
SI_USBXPRESS_FLUSH_BUFFERS
,
SI_USBXPRESS_GET_VERSION
,
SI_USBXPRESS_NOT_CLEAR_TO_SEND
,
SI_USBXPRESS_REQUEST
,
USB_Setup_TypeDef::Type
,
USB_SETUP_DIR_D2H
,
USB_SETUP_RECIPIENT_DEVICE
,
USB_SETUP_RECIPIENT_INTERFACE
,
USB_SETUP_TYPE_STANDARD
,
USB_SETUP_TYPE_VENDOR
,
USB_SETUP_TYPE_VENDOR_MASK
,
USB_STATUS_OK
,
USB_STATUS_REQ_UNHANDLED
,
USB_STRING_DESCRIPTOR
,
USBD_AbortTransfer()
,
USBD_Write()
,
USBX_DEV_CLOSE
,
USBX_DEV_OPEN
,
USBX_FIFO_PURGE
,
USBX_jumpCallback()
,
USBXCORE_apiEa
,
USBXCORE_apiIntValue
,
USBXCORE_resetState()
,
USB_Setup_TypeDef::wIndex
,
USB_Setup_TypeDef::wLength
, and
USB_Setup_TypeDef::wValue
.
Referenced by USBX_init() .