BATTERY_TypeDef Struct Reference

Defines segment COM and BIT fields for Battery (suited for Anim)

Definition at line 98 of file segmentlcd.c .

Data Fields

uint8_t bit [4]
uint8_t com [4]

Field Documentation

uint8_t BATTERY_TypeDef::bit[4]

LCD bit number

Definition at line 100 of file segmentlcd.c .

Referenced by SegmentLCD_Battery() .

uint8_t BATTERY_TypeDef::com[4]

LCD COM line (for multiplexing)

Definition at line 99 of file segmentlcd.c .

Referenced by SegmentLCD_Battery() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/hardware/kit/common/drivers/ segmentlcd.c