ACMP_VBConfig_TypeDef Struct ReferenceEMLIB > ACMP
VB Configuration structure. This structure is used to configure the VB voltage input source and its dividers.
       Definition at line
       
        907
       
       of file
       
        em_acmp.h
       
       .
      
      
       #include <
       
     
        em_acmp.h
       
       >
      
         Data Fields | 
       |
| uint32_t | div0 | 
| uint32_t | div1 | 
| ACMP_VBInput_TypeDef | input | 
Field Documentation
| uint32_t ACMP_VBConfig_TypeDef::div0 | 
A divider for VB voltage input source when ACMP output is 0. This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.
VB divided = VB input * (div0 + 1) / 64
        Definition at line
        
         917
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_VBSetup() .
| uint32_t ACMP_VBConfig_TypeDef::div1 | 
A divider for VB voltage input source when ACMP output is 1. This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.
VB divided = VB input * (div1 + 1) / 64
        Definition at line
        
         926
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_VBSetup() .
| ACMP_VBInput_TypeDef ACMP_VBConfig_TypeDef::input | 
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/platform/emlib/inc/
       
em_acmp.h