QSPI_DelayConfig_TypeDef Struct ReferenceEMLIB > QSPI
QSPI Device Delay Configuration Structure.
Definition at line
149
of file
em_qspi.h
.
#include <
em_qspi.h
>
Data Fields |
|
| uint8_t | deassert |
| uint8_t | deviceSwitch |
| uint8_t | firstBit |
| uint8_t | lastBit |
Field Documentation
| uint8_t QSPI_DelayConfig_TypeDef::deassert |
The minimal delay to keep the chip select line de-asserted between two transactions.
Definition at line
152
of file
em_qspi.h
.
| uint8_t QSPI_DelayConfig_TypeDef::deviceSwitch |
Delay between one chip select being de-activated and the activation of another.
Definition at line
156
of file
em_qspi.h
.
| uint8_t QSPI_DelayConfig_TypeDef::firstBit |
Delay chip select assert and first bit in a transaction.
Definition at line
162
of file
em_qspi.h
.
| uint8_t QSPI_DelayConfig_TypeDef::lastBit |
Delay between last bit and chip select de-assert.
Definition at line
159
of file
em_qspi.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_qspi.h