RTCC_Init_TypeDef Struct ReferenceEMLIB > RTCC
RTCC initialization structure.
Definition at line 214
of file em_rtcc.h
.
#include <
em_rtcc.h
>
Data Fields | |
RTCC_CntMode_TypeDef | cntMode |
bool | cntWrapOnCCV1 |
bool | debugRun |
bool | disLeapYearCorr |
bool | enaBackupModeSet |
bool | enable |
bool | enaOSCFailDetect |
bool | precntWrapOnCCV0 |
RTCC_CntPresc_TypeDef | presc |
RTCC_PrescMode_TypeDef | prescMode |
Field Documentation
RTCC_CntMode_TypeDef RTCC_Init_TypeDef::cntMode |
Select operational mode of the counter.
Definition at line 247
of file em_rtcc.h
.
Referenced by RTCC_Init().
bool RTCC_Init_TypeDef::cntWrapOnCCV1 |
Enable/disable counter wrap on ch. 1 CCV value.
Definition at line 225
of file em_rtcc.h
.
Referenced by RTCC_Init().
bool RTCC_Init_TypeDef::debugRun |
Enable/disable timer counting during debug halt.
Definition at line 219
of file em_rtcc.h
.
Referenced by RTCC_Init().
bool RTCC_Init_TypeDef::disLeapYearCorr |
Disable leap year correction for calendar mode. When this parameter is set to false, February has 29 days if (year % 4 == 0). If set to true, February always has 28 days.
Definition at line 254
of file em_rtcc.h
.
Referenced by RTCC_Init().
bool RTCC_Init_TypeDef::enaBackupModeSet |
Enable/disable storing RTCC counter value in RTCC_CCV2 upon backup mode entry.
Definition at line 236
of file em_rtcc.h
.
Referenced by RTCC_Init().
bool RTCC_Init_TypeDef::enable |
Enable/disable counting when initialization is completed.
Definition at line 216
of file em_rtcc.h
.
Referenced by RTCC_Init().
bool RTCC_Init_TypeDef::enaOSCFailDetect |
Enable/disable the check that sets OSCFFAIL interrupt flag if no LFCLK-RTCC ticks are detected within one ULFRCO cycles.
Definition at line 242
of file em_rtcc.h
.
Referenced by RTCC_Init().
bool RTCC_Init_TypeDef::precntWrapOnCCV0 |
Enable/disable pre-counter wrap on ch. 0 CCV value.
Definition at line 222
of file em_rtcc.h
.
Referenced by RTCC_Init().
RTCC_CntPresc_TypeDef RTCC_Init_TypeDef::presc |
Counter prescaler.
Definition at line 228
of file em_rtcc.h
.
Referenced by RTCC_Init(), and RTCDRV_Init().
RTCC_PrescMode_TypeDef RTCC_Init_TypeDef::prescMode |
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emlib/inc/
em_rtcc.h