CMU_LFXOInit_TypeDef Struct ReferenceEMLIB > CMU
LFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.
Definition at line
2136
of file
em_cmu.h
.
#include <
em_cmu.h
>
Data Fields |
|
| uint8_t | ctune |
| uint8_t | gain |
| CMU_OscMode_TypeDef | mode |
| uint8_t | timeout |
Field Documentation
| uint8_t CMU_LFXOInit_TypeDef::ctune |
CTUNE (load capacitance) value
Definition at line
2138
of file
em_cmu.h
.
Referenced by BSP_initClocks() , and CMU_LFXOInit() .
| uint8_t CMU_LFXOInit_TypeDef::gain |
| CMU_OscMode_TypeDef CMU_LFXOInit_TypeDef::mode |
| uint8_t CMU_LFXOInit_TypeDef::timeout |
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_cmu.h