SDIO_TypeDef Struct ReferenceDevices > SDIO
SDIO Register Declaration
Definition at line
48
of file
efm32gg11b_sdio.h
.
#include <
efm32gg11b_sdio.h
>
Data Fields |
|
| __IOM uint32_t | AC12ERRSTAT |
| __IM uint32_t | ADMAES |
| __IOM uint32_t | ADSADDR |
| __IOM uint32_t | BLKSIZE |
| __IOM uint32_t | BOOTTOCTRL |
| __IOM uint32_t | BUFDATPORT |
| __IM uint32_t | CAPAB0 |
| __IM uint32_t | CAPAB2 |
| __IOM uint32_t | CFG0 |
| __IOM uint32_t | CFG1 |
| __IOM uint32_t | CFGPRESETVAL0 |
| __IOM uint32_t | CFGPRESETVAL1 |
| __IOM uint32_t | CFGPRESETVAL2 |
| __IOM uint32_t | CFGPRESETVAL3 |
| __IOM uint32_t | CLOCKCTRL |
| __IOM uint32_t | CMDARG1 |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | FEVTERRSTAT |
| __IOM uint32_t | HOSTCTRL1 |
| __IOM uint32_t | IEN |
| __IOM uint32_t | IFCR |
| __IOM uint32_t | IFENC |
| __IM uint32_t | MAXCURCAPAB |
| __IM uint32_t | PRSSTAT |
| __IM uint32_t | PRSTVAL0 |
| __IM uint32_t | PRSTVAL2 |
| __IM uint32_t | PRSTVAL4 |
| __IM uint32_t | PRSTVAL6 |
| uint32_t | RESERVED0 [1U] |
| uint32_t | RESERVED1 [1U] |
| uint32_t | RESERVED2 [34U] |
| uint32_t | RESERVED3 [448U] |
| __IM uint32_t | RESP0 |
| __IM uint32_t | RESP2 |
| __IM uint32_t | RESP4 |
| __IM uint32_t | RESP6 |
| __IOM uint32_t | ROUTELOC0 |
| __IOM uint32_t | ROUTELOC1 |
| __IOM uint32_t | ROUTEPEN |
| __IOM uint32_t | SDMASYSADDR |
| __IM uint32_t | SLOTINTSTAT |
| __IOM uint32_t | TFRMODE |
Field Documentation
| __IOM uint32_t SDIO_TypeDef::AC12ERRSTAT |
AUTO CMD12 Error Status and Host Control2 Register
Definition at line
64
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::ADMAES |
ADMA Error Status Register
Definition at line
70
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::ADSADDR |
ADMA System Address Register
Definition at line
71
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::BLKSIZE |
Block Size and Block Count Register
Definition at line
50
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::BOOTTOCTRL |
Boot Timeout Control Register
Definition at line
77
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::BUFDATPORT |
Buffer Data Register
Definition at line
57
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::CAPAB0 |
Capabilities Register to Hold Bits 31~0
Definition at line
65
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::CAPAB2 |
Capabilities Register to Hold Bits 63~32
Definition at line
66
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::CFG0 |
Core Configuration 0
Definition at line
83
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::CFG1 |
Core Configuration 1
Definition at line
84
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::CFGPRESETVAL0 |
Core Configuration Preset Value 0
Definition at line
85
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::CFGPRESETVAL1 |
Core Configuration Preset Value 1
Definition at line
86
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::CFGPRESETVAL2 |
Core Configuration Preset Value 2
Definition at line
87
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::CFGPRESETVAL3 |
Core Configuration Preset Value 3
Definition at line
88
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::CLOCKCTRL |
Clock Control, Timeout Control and Software Register
Definition at line
60
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::CMDARG1 |
SD Command Argument Register
Definition at line
51
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::CTRL |
Core Control Signals
Definition at line
82
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::FEVTERRSTAT |
Force Event Register for Auto CMD Error Status
Definition at line
69
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::HOSTCTRL1 |
Host Control1, Power, Block Gap and Wakeup-up Control Register
Definition at line
59
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::IEN |
Normal and Error Interrupt Signal Enable Register
Definition at line
63
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::IFCR |
Normal and Error Interrupt Status Register
Definition at line
61
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::IFENC |
Normal and Error Interrupt Status Enable Register
Definition at line
62
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::MAXCURCAPAB |
Maximum Current Capabilities Register
Definition at line
67
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::PRSSTAT |
Present State Register
Definition at line
58
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::PRSTVAL0 |
Preset Value for Initialization and Default Speed Mode
Definition at line
73
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::PRSTVAL2 |
Preset Value for High Speed and SDR12 Modes
Definition at line
74
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::PRSTVAL4 |
Preset Value for SDR25 and SDR50 Modes
Definition at line
75
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::PRSTVAL6 |
Preset Value for SDR104 and DDR50 Modes
Definition at line
76
of file
efm32gg11b_sdio.h
.
| uint32_t SDIO_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
68
of file
efm32gg11b_sdio.h
.
| uint32_t SDIO_TypeDef::RESERVED1[1U] |
Reserved for future use
Definition at line
72
of file
efm32gg11b_sdio.h
.
| uint32_t SDIO_TypeDef::RESERVED2[34U] |
Reserved for future use
Definition at line
78
of file
efm32gg11b_sdio.h
.
| uint32_t SDIO_TypeDef::RESERVED3[448U] |
Reserved for future use
Definition at line
81
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::RESP0 |
Response0 and Response1 Register
Definition at line
53
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::RESP2 |
Response2 and Response3 Register
Definition at line
54
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::RESP4 |
Response4 and Response5 Register
Definition at line
55
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::RESP6 |
Response6 and Response7 Register
Definition at line
56
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::ROUTELOC0 |
I/O LOCATION Register
Definition at line
89
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::ROUTELOC1 |
I/O LOCATION Register
Definition at line
90
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::ROUTEPEN |
I/O LOCATION Enable Register
Definition at line
91
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::SDMASYSADDR |
SDMA System Address Register
Definition at line
49
of file
efm32gg11b_sdio.h
.
| __IM uint32_t SDIO_TypeDef::SLOTINTSTAT |
Slot Interrupt Status Register
Definition at line
79
of file
efm32gg11b_sdio.h
.
| __IOM uint32_t SDIO_TypeDef::TFRMODE |
Transfer Mode and Command Register
Definition at line
52
of file
efm32gg11b_sdio.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/
efm32gg11b_sdio.h