CRYOTIMER_TypeDef Struct ReferenceDevices > CRYOTIMER
CRYOTIMER Register Declaration
Definition at line
48
of file
efm32gg11b_cryotimer.h
.
#include <
efm32gg11b_cryotimer.h
>
Data Fields |
|
| __IM uint32_t | CNT |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | EM4WUEN |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | PERIODSEL |
Field Documentation
| __IM uint32_t CRYOTIMER_TypeDef::CNT |
Counter Value
Definition at line
51
of file
efm32gg11b_cryotimer.h
.
| __IOM uint32_t CRYOTIMER_TypeDef::CTRL |
Control Register
Definition at line
49
of file
efm32gg11b_cryotimer.h
.
| __IOM uint32_t CRYOTIMER_TypeDef::EM4WUEN |
Wake Up Enable
Definition at line
52
of file
efm32gg11b_cryotimer.h
.
| __IOM uint32_t CRYOTIMER_TypeDef::IEN |
Interrupt Enable Register
Definition at line
56
of file
efm32gg11b_cryotimer.h
.
| __IM uint32_t CRYOTIMER_TypeDef::IF |
Interrupt Flag Register
Definition at line
53
of file
efm32gg11b_cryotimer.h
.
| __IOM uint32_t CRYOTIMER_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
55
of file
efm32gg11b_cryotimer.h
.
| __IOM uint32_t CRYOTIMER_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
54
of file
efm32gg11b_cryotimer.h
.
| __IOM uint32_t CRYOTIMER_TypeDef::PERIODSEL |
Interrupt Duration
Definition at line
50
of file
efm32gg11b_cryotimer.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/
efm32gg11b_cryotimer.h