Direct_Receive_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Direct receive plugin, see Plugin System Layer for detailed documentation.
.
         Data Structures | 
       |
| struct | EZRADIODRV_DirectRxHandle | 
| 
         EzRadio direct rx plug-in instance initialization and handler structure.
          | 
       |
         Macros | 
       |
| #define | EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT | 
| 
         Configuration data for EzRadio direct rx plug-in.
          | 
       |
         Typedefs | 
       |
| typedef struct EZRADIODRV_DirectRxHandle | EZRADIODRV_DirectRxHandle_t | 
| 
         EzRadio direct rx plug-in instance initialization and handler structure.
          | 
       |
         Functions | 
       |
| Ecode_t | ezradioStartDirectReceive ( EZRADIODRV_Handle_t radioHandle) | 
| 
         Starts direct reception with the radio configurations from the radioHandle parameter.
          | 
       |
| Ecode_t | ezradioStopDirectReceive (void) | 
| 
         Stops direct reception.
          | 
       |
Macro Definition Documentation
| #define EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT | 
Configuration data for EzRadio direct rx plug-in.
        Definition at line
        
         58
        
        of file
        
         ezradio_direct_receive_plugin.h
        
        .
       
Function Documentation
| Ecode_t ezradioStartDirectReceive | ( | EZRADIODRV_Handle_t | 
           
            radioHandle
           
           | 
          ) | 
Starts direct reception with the radio configurations from the radioHandle parameter.
- Parameters
 - 
         
radioHandleHandler of the EzRadio driver instance where channel configuration is set.  
- Returns
 - ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
 
        Definition at line
        
         41
        
        of file
        
         ezradio_direct_receive_plugin.c
        
        .
       
References EZRADIODRV_DirectRxHandle::channel , EZRADIODRV_HandleData::directRx , ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradio_get_int_status() , and ezradio_start_rx() .
| Ecode_t ezradioStopDirectReceive | ( | void | 
           
           
           | 
          ) | 
Stops direct reception.
- Returns
 - ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
 
        Definition at line
        
         66
        
        of file
        
         ezradio_direct_receive_plugin.c
        
        .
       
References ECODE_EMDRV_EZRADIODRV_OK , and ezradio_change_state() .