UARTDRV_InitLeuart_t Struct ReferenceEMDRV > UARTDRV
LEUART driver instance initialization structure. Contains a number of UARTDRV configuration options. It is required to initialize a driver instance. This structure is passed to UARTDRV_InitLeuart() when initializing a UARTDRV instance.
       Definition at line
       
        219
       
       of file
       
        uartdrv.h
       
       .
      
      
       #include <
       
     
        uartdrv.h
       
       >
      
         Data Fields | 
       |
| uint32_t | baudRate | 
| 
         UART baud rate.
          | 
       |
| uint8_t | ctsPin | 
| 
         CTS pin number.
          | 
       |
| GPIO_Port_TypeDef | ctsPort | 
| 
         CTS pin port number.
          | 
       |
| UARTDRV_FlowControlType_t | fcType | 
| 
         Flow control mode.
          | 
       |
| LEUART_Parity_TypeDef | parity | 
| 
         Parity configuration.
          | 
       |
| LEUART_TypeDef * | port | 
| 
         The peripheral used for LEUART.
          | 
       |
| uint8_t | portLocationRx | 
| 
         Location number for LEUART Rx pin.
          | 
       |
| uint8_t | portLocationTx | 
| 
         Location number for LEUART Tx pin.
          | 
       |
| uint8_t | rtsPin | 
| 
         RTS pin number.
          | 
       |
| GPIO_Port_TypeDef | rtsPort | 
| 
         RTS pin port number.
          | 
       |
| UARTDRV_Buffer_FifoQueue_t * | rxQueue | 
| 
         Receive operation queue.
          | 
       |
| LEUART_Stopbits_TypeDef | stopBits | 
| 
         Number of stop bits.
          | 
       |
| UARTDRV_Buffer_FifoQueue_t * | txQueue | 
| 
         Transmit operation queue.
          | 
       |
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/platform/emdrv/uartdrv/inc/
       
uartdrv.h