ARING_TypeDef Struct ReferenceKit Drivers > SegmentLcd
Defines segment COM and BIT fields for A-wheel (suited for Anim)
       Definition at line
       
        107
       
       of file
       
        segmentlcd.c
       
       .
      
         Data Fields | 
       |
| uint8_t | bit [8] | 
| uint8_t | com [8] | 
Field Documentation
| uint8_t ARING_TypeDef::bit[8] | 
LCD bit number
        Definition at line
        
         109
        
        of file
        
         segmentlcd.c
        
        .
       
| uint8_t ARING_TypeDef::com[8] | 
LCD COM line (for multiplexing)
        Definition at line
        
         108
        
        of file
        
         segmentlcd.c
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/hardware/kit/common/drivers/
       
segmentlcd.c