LETIMEREMLIB
Detailed Description
Low Energy Timer (LETIMER) Peripheral API.
This module contains functions to control the LETIMER peripheral of Silicon Labs 32-bit MCUs and SoCs. The LETIMER is a down-counter that can keep track of time and output configurable waveforms.
         Data Structures | 
       |
| struct | LETIMER_Init_TypeDef | 
         Macros | 
       |
| #define | LETIMER_INIT_DEFAULT | 
         Enumerations | 
       |
| enum | 
         
          LETIMER_RepeatMode_TypeDef
         
         {
          letimerRepeatFree = _LETIMER_CTRL_REPMODE_FREE, letimerRepeatOneshot = _LETIMER_CTRL_REPMODE_ONESHOT, letimerRepeatBuffered = _LETIMER_CTRL_REPMODE_BUFFERED, letimerRepeatDouble = _LETIMER_CTRL_REPMODE_DOUBLE }  | 
       
| enum | 
         
          LETIMER_UFOA_TypeDef
         
         {
          letimerUFOANone = _LETIMER_CTRL_UFOA0_NONE, letimerUFOAToggle = _LETIMER_CTRL_UFOA0_TOGGLE, letimerUFOAPulse = _LETIMER_CTRL_UFOA0_PULSE, letimerUFOAPwm = _LETIMER_CTRL_UFOA0_PWM }  | 
       
         Functions | 
       |
| uint32_t | LETIMER_CompareGet ( LETIMER_TypeDef *letimer, unsigned int comp) | 
| 
         Get the LETIMER compare register value.
          | 
       |
| void | LETIMER_CompareSet ( LETIMER_TypeDef *letimer, unsigned int comp, uint32_t value) | 
| 
         Set the LETIMER compare register value.
          | 
       |
| __STATIC_INLINE uint32_t | LETIMER_CounterGet ( LETIMER_TypeDef *letimer) | 
| 
         Get LETIMER counter value.
          | 
       |
| void | LETIMER_Enable ( LETIMER_TypeDef *letimer, bool enable) | 
| 
         Start/stop LETIMER.
          | 
       |
| void | LETIMER_Init ( LETIMER_TypeDef *letimer, const LETIMER_Init_TypeDef *init) | 
| 
         Initialize LETIMER.
          | 
       |
| __STATIC_INLINE void | LETIMER_IntClear ( LETIMER_TypeDef *letimer, uint32_t flags) | 
| 
         Clear one or more pending LETIMER interrupts.
          | 
       |
| __STATIC_INLINE void | LETIMER_IntDisable ( LETIMER_TypeDef *letimer, uint32_t flags) | 
| 
         Disable one or more LETIMER interrupts.
          | 
       |
| __STATIC_INLINE void | LETIMER_IntEnable ( LETIMER_TypeDef *letimer, uint32_t flags) | 
| 
         Enable one or more LETIMER interrupts.
          | 
       |
| __STATIC_INLINE uint32_t | LETIMER_IntGet ( LETIMER_TypeDef *letimer) | 
| 
         Get pending LETIMER interrupt flags.
          | 
       |
| __STATIC_INLINE uint32_t | LETIMER_IntGetEnabled ( LETIMER_TypeDef *letimer) | 
| 
         Get enabled and pending LETIMER interrupt flags.
          | 
       |
| __STATIC_INLINE void | LETIMER_IntSet ( LETIMER_TypeDef *letimer, uint32_t flags) | 
| 
         Set one or more pending LETIMER interrupts from SW.
          | 
       |
| uint32_t | LETIMER_RepeatGet ( LETIMER_TypeDef *letimer, unsigned int rep) | 
| 
         Get the LETIMER repeat register value.
          | 
       |
| void | LETIMER_RepeatSet ( LETIMER_TypeDef *letimer, unsigned int rep, uint32_t value) | 
| 
         Set the LETIMER repeat counter register value.
          | 
       |
| void | LETIMER_Reset ( LETIMER_TypeDef *letimer) | 
| 
         Reset LETIMER to the same state that it was in after a hardware reset.
          | 
       |
| void | LETIMER_SyncWait ( LETIMER_TypeDef *letimer) | 
| 
         Wait for the LETIMER to complete all synchronization of register changes and commands.
          | 
       |
| __STATIC_INLINE uint32_t | LETIMER_TopGet ( LETIMER_TypeDef *letimer) | 
| 
         Get the current LETIMER top value.
          | 
       |
| void | LETIMER_TopSet ( LETIMER_TypeDef *letimer, uint32_t value) | 
| 
         Set the LETIMER top value.
          | 
       |
Macro Definition Documentation
| #define LETIMER_INIT_DEFAULT | 
Default configuration for LETIMER initialization structure.
        Definition at line
        
         127
        
        of file
        
         em_letimer.h
        
        .
       
Referenced by MIC_init() .
Enumeration Type Documentation
Repeat mode.
        Definition at line
        
         58
        
        of file
        
         em_letimer.h
        
        .
       
| enum LETIMER_UFOA_TypeDef | 
Underflow action on output.
        Definition at line
        
         76
        
        of file
        
         em_letimer.h
        
        .
       
Function Documentation
| uint32_t LETIMER_CompareGet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| unsigned int | 
           
            comp
           
           | 
         ||
| ) | 
Get the LETIMER compare register value.
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] compA compare register to get, either 0 or 1.  
- Returns
 - A compare register value, 0 if invalid register selected.
 
        Definition at line
        
         134
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_TypeDef::COMP0 , and LETIMER_TypeDef::COMP1 .
| void LETIMER_CompareSet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| unsigned int | 
           
            comp,
           
           | 
         ||
| uint32_t | 
           
            value
           
           | 
         ||
| ) | 
Set the LETIMER compare register value.
- Note
 - The setting of a compare register requires synchronization into the low frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
 
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] compA compare register to set, either 0 or 1. [in] valueAn initialization value (<= 0x0000ffff).  
        Definition at line
        
         179
        
        of file
        
         em_letimer.c
        
        .
       
References _LETIMER_COMP0_COMP0_MASK , _LETIMER_COMP0_COMP0_SHIFT , LETIMER_TypeDef::COMP0 , and LETIMER_TypeDef::COMP1 .
Referenced by LETIMER_TopSet() , and MIC_init() .
| __STATIC_INLINE uint32_t LETIMER_CounterGet | ( | LETIMER_TypeDef * | 
           
            letimer
           
           | 
          ) | 
Get LETIMER counter value.
- Parameters
 - 
         
[in] letimerPointer to the LETIMER peripheral register block.  
- Returns
 - Current LETIMER counter value.
 
        Definition at line
        
         161
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::CNT .
| void LETIMER_Enable | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| bool | 
           
            enable
           
           | 
         ||
| ) | 
Start/stop LETIMER.
- Note
 - The enabling/disabling of the LETIMER modifies the LETIMER CMD register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
 
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] enableTrue to enable counting, false to disable.  
        Definition at line
        
         232
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_TypeDef::CMD , LETIMER_CMD_START , LETIMER_CMD_STOP , LETIMER_SYNCBUSY_CMD , and LETIMER_TypeDef::SYNCBUSY .
| void LETIMER_Init | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| const LETIMER_Init_TypeDef * | 
           
            init
           
           | 
         ||
| ) | 
Initialize LETIMER.
Note that the compare/repeat values must be set separately with LETIMER_CompareSet() and LETIMER_RepeatSet() . That should probably be done prior using this function if configuring the LETIMER to start when initialization is complete.
- Note
 - The initialization of the LETIMER modifies the LETIMER CTRL/CMD registers which require synchronization into the low-frequency domain. If any of those registers are modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
 
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] initA pointer to the LETIMER initialization structure.  
        Definition at line
        
         326
        
        of file
        
         em_letimer.c
        
        .
       
References _LETIMER_CTRL_REPMODE_SHIFT , _LETIMER_CTRL_UFOA0_SHIFT , _LETIMER_CTRL_UFOA1_SHIFT , LETIMER_Init_TypeDef::bufTop , LETIMER_TypeDef::CMD , LETIMER_TypeDef::COMP0 , LETIMER_Init_TypeDef::comp0Top , LETIMER_TypeDef::CTRL , LETIMER_Init_TypeDef::debugRun , LETIMER_Init_TypeDef::enable , LETIMER_CMD_START , LETIMER_CMD_STOP , LETIMER_CTRL_BUFTOP , LETIMER_CTRL_COMP0TOP , LETIMER_CTRL_DEBUGRUN , LETIMER_CTRL_OPOL0 , LETIMER_CTRL_OPOL1 , LETIMER_STATUS_RUNNING , LETIMER_SYNCBUSY_CMD , LETIMER_Init_TypeDef::out0Pol , LETIMER_Init_TypeDef::out1Pol , LETIMER_Init_TypeDef::repMode , LETIMER_TypeDef::STATUS , LETIMER_TypeDef::SYNCBUSY , LETIMER_Init_TypeDef::topValue , LETIMER_Init_TypeDef::ufoa0 , and LETIMER_Init_TypeDef::ufoa1 .
Referenced by MIC_init() .
| __STATIC_INLINE void LETIMER_IntClear | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Clear one or more pending LETIMER interrupts.
- Parameters
 - 
         
[in] letimerPointer to LETIMER peripheral register block. [in] flagsPending LETIMER interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).  
        Definition at line
        
         184
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IFC .
Referenced by LETIMER_Reset() .
| __STATIC_INLINE void LETIMER_IntDisable | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Disable one or more LETIMER interrupts.
- Parameters
 - 
         
[in] letimerPointer to LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).  
        Definition at line
        
         204
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IEN .
| __STATIC_INLINE void LETIMER_IntEnable | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Enable one or more LETIMER interrupts.
- Note
 - Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using LETIMER_IntClear() prior to enabling the interrupt.
 
- Parameters
 - 
         
[in] letimerPointer to the LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).  
        Definition at line
        
         225
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IEN .
| __STATIC_INLINE uint32_t LETIMER_IntGet | ( | LETIMER_TypeDef * | 
           
            letimer
           
           | 
          ) | 
Get pending LETIMER interrupt flags.
- Note
 - Event bits are not cleared by the use of this function.
 
- Parameters
 - 
         
[in] letimerPointer to LETIMER peripheral register block.  
- Returns
 - LETIMER interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
 
        Definition at line
        
         244
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IF .
| __STATIC_INLINE uint32_t LETIMER_IntGetEnabled | ( | LETIMER_TypeDef * | 
           
            letimer
           
           | 
          ) | 
Get enabled and pending LETIMER interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
 - Event bits are not cleared by the use of this function.
 
- Parameters
 - 
         
[in] letimerPointer to LETIMER peripheral register block.  
- Returns
 - 
         Pending and enabled LETIMER interrupt sources. Return value is the bitwise AND combination of
         
- the OR combination of enabled interrupt sources in LETIMER_IEN_nnn register (LETIMER_IEN_nnn) and
 - the OR combination of valid interrupt flags of the LETIMER module (LETIMER_IF_nnn).
 
 
        Definition at line
        
         270
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IEN , and LETIMER_TypeDef::IF .
| __STATIC_INLINE void LETIMER_IntSet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Set one or more pending LETIMER interrupts from SW.
- Parameters
 - 
         
[in] letimerPointer to LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).  
        Definition at line
        
         293
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IFS .
| uint32_t LETIMER_RepeatGet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| unsigned int | 
           
            rep
           
           | 
         ||
| ) | 
Get the LETIMER repeat register value.
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] repRepeat register to get, either 0 or 1.  
- Returns
 - Repeat register value, 0 if invalid register selected.
 
        Definition at line
        
         422
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_TypeDef::REP0 , and LETIMER_TypeDef::REP1 .
| void LETIMER_RepeatSet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| unsigned int | 
           
            rep,
           
           | 
         ||
| uint32_t | 
           
            value
           
           | 
         ||
| ) | 
Set the LETIMER repeat counter register value.
- Note
 - The setting of a repeat counter register requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
 
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] repRepeat counter register to set, either 0 or 1. [in] valueAn initialization value (<= 0x0000ffff).  
        Definition at line
        
         467
        
        of file
        
         em_letimer.c
        
        .
       
References _LETIMER_REP0_REP0_MASK , _LETIMER_REP0_REP0_SHIFT , LETIMER_TypeDef::REP0 , and LETIMER_TypeDef::REP1 .
Referenced by MIC_init() .
| void LETIMER_Reset | ( | LETIMER_TypeDef * | 
           
            letimer
           
           | 
          ) | 
Reset LETIMER to the same state that it was in after a hardware reset.
- Note
 - The ROUTE register is NOT reset by this function to allow for a centralized setup of this feature.
 
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block.  
        Definition at line
        
         521
        
        of file
        
         em_letimer.c
        
        .
       
References _LETIMER_COMP0_RESETVALUE , _LETIMER_COMP1_RESETVALUE , _LETIMER_CTRL_RESETVALUE , _LETIMER_IEN_RESETVALUE , _LETIMER_IF_MASK , _LETIMER_REP0_RESETVALUE , _LETIMER_REP1_RESETVALUE , _LETIMER_SYNCBUSY_MASK , LETIMER_TypeDef::CMD , LETIMER_TypeDef::COMP0 , LETIMER_TypeDef::COMP1 , LETIMER_TypeDef::CTRL , LETIMER_TypeDef::IEN , LETIMER0 , LETIMER_CMD_CLEAR , LETIMER_CMD_CTO0 , LETIMER_CMD_CTO1 , LETIMER_CMD_STOP , LETIMER_IntClear() , LETIMER_TypeDef::REP0 , and LETIMER_TypeDef::REP1 .
| __STATIC_INLINE uint32_t LETIMER_TopGet | ( | LETIMER_TypeDef * | 
           
            letimer
           
           | 
          ) | 
Get the current LETIMER top value.
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block.  
- Returns
 - The top value. This will be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices.
 
        Definition at line
        
         321
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::COMP0 .
| void LETIMER_TopSet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| uint32_t | 
           
            value
           
           | 
         ||
| ) | 
Set the LETIMER top value.
- Note
 - The LETIMER is a down-counter, so when the counter reaches 0 then the top value will be loaded into the counter. This function can be used to set the top value.
 
If the LETIMER is not already configured to use a top value then this function will enable that functionality for the user.
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] valueThe top value. This can be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices.  
        Definition at line
        
         591
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_TypeDef::CTRL , LETIMER_CompareSet() , LETIMER_CTRL_COMP0TOP , and LETIMER_SyncWait() .