ACMP_Init_TypeDef Struct ReferenceEMLIB > ACMP
ACMP initialization structure.
       Definition at line
       
        733
       
       of file
       
        em_acmp.h
       
       .
      
      
       #include <
       
     
        em_acmp.h
       
       >
      
Field Documentation
| ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy | 
ACMP accuracy mode. Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.
        Definition at line
        
         771
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
| uint32_t ACMP_Init_TypeDef::biasProg | 
Bias current. See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
        Definition at line
        
         748
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
| bool ACMP_Init_TypeDef::enable | 
If true, ACMP is enabled after configuration.
        Definition at line
        
         823
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
| bool ACMP_Init_TypeDef::fullBias | 
Full-bias current. See the ACMP chapter about bias and response time in the reference manual for details.
        Definition at line
        
         737
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
| ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_0 | 
Hysteresis when ACMP output is 0.
        Definition at line
        
         791
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
| ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_1 | 
Hysteresis when ACMP output is 1.
        Definition at line
        
         794
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
| bool ACMP_Init_TypeDef::inactiveValue | 
Inactive value emitted by ACMP during warmup.
        Definition at line
        
         804
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
| ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange | 
Input range. Adjust this setting to optimize the performance for a given input voltage range.
        Definition at line
        
         763
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
| bool ACMP_Init_TypeDef::interruptOnFallingEdge | 
Enable setting the interrupt flag on the falling edge.
        Definition at line
        
         752
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
| bool ACMP_Init_TypeDef::interruptOnRisingEdge | 
Enable setting the interrupt flag on the rising edge.
        Definition at line
        
         756
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
| ACMP_PowerSource_TypeDef ACMP_Init_TypeDef::powerSource | 
Select the power source for the ACMP.
        Definition at line
        
         776
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
| ACMP_VLPInput_Typedef ACMP_Init_TypeDef::vlpInput | 
VLP Input source. Select between using VADIV or VBDIV as the VLP source.
        Definition at line
        
         800
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/platform/emlib/inc/
       
em_acmp.h