MSDD_CmdStatus_TypeDef Struct ReferenceKit Drivers > Gecko USB MSD
Status info for one BOT CBW -> Data I/O -> CSW cycle.
Definition at line
39
of file
msdd.h
.
#include <
msdd.h
>
Public Types |
|
enum |
{
XFER_MEMORYMAPPED = 0, XFER_INDIRECT } |
Data Fields |
|
uint8_t | direction |
uint32_t | lba |
uint32_t | maxBurst |
uint8_t * | pData |
bool | valid |
uint32_t | xferLen |
enum MSDD_CmdStatus_TypeDef:: { ... } | xferType |
Field Documentation
uint8_t MSDD_CmdStatus_TypeDef::direction |
Set if BOT direction is IN.
Definition at line
41
of file
msdd.h
.
uint32_t MSDD_CmdStatus_TypeDef::lba |
SCSI Read/Write lba address.
Definition at line
43
of file
msdd.h
.
uint32_t MSDD_CmdStatus_TypeDef::maxBurst |
Max length of one transfer.
Definition at line
45
of file
msdd.h
.
uint8_t* MSDD_CmdStatus_TypeDef::pData |
Media data pointer.
Definition at line
42
of file
msdd.h
.
bool MSDD_CmdStatus_TypeDef::valid |
True if the CBW is valid.
Definition at line
40
of file
msdd.h
.
uint32_t MSDD_CmdStatus_TypeDef::xferLen |
BOT transfer length.
Definition at line
44
of file
msdd.h
.
enum { ... } MSDD_CmdStatus_TypeDef::xferType |
MSD media access type.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/hardware/kit/common/drivers/
msdd.h