BCP_PacketHeader Struct ReferenceBSP > API for STKs and WSTKs

BCP Packet Header definition.

Definition at line 101 of file bsp_bcp.h .

#include < bsp_bcp.h >

Data Fields

uint8_t magic
uint8_t payloadLength
uint8_t reserved
uint8_t type

Field Documentation

uint8_t BCP_PacketHeader::magic

Magic - start of packet - must be BSP_BCP_MAGIC

Definition at line 102 of file bsp_bcp.h .

uint8_t BCP_PacketHeader::payloadLength

Length of data segment >=0 and <=BSP_BCP_PACKET_SIZE

Definition at line 104 of file bsp_bcp.h .

uint8_t BCP_PacketHeader::reserved

Reserved for future expansion

Definition at line 105 of file bsp_bcp.h .

uint8_t BCP_PacketHeader::type

Type - packet type

Definition at line 103 of file bsp_bcp.h .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/hardware/kit/common/bsp/ bsp_bcp.h