CAN_Init_TypeDef Struct ReferenceEMLIB > CAN
CAN initialization structure.
Definition at line
155
of file
em_can.h
.
#include <
em_can.h
>
Data Fields |
|
uint32_t | bitrate |
bool | enable |
uint8_t | phaseBufferSegment1 |
uint8_t | phaseBufferSegment2 |
uint8_t | propagationTimeSegment |
bool | resetMessages |
uint8_t | synchronisationJumpWidth |
Field Documentation
uint32_t CAN_Init_TypeDef::bitrate |
bool CAN_Init_TypeDef::enable |
True to set the CAN Device in normal mode after initialization.
Definition at line
157
of file
em_can.h
.
Referenced by CAN_Init() .
uint8_t CAN_Init_TypeDef::phaseBufferSegment1 |
Default Phase Buffer Segment 1.
Definition at line
169
of file
em_can.h
.
Referenced by CAN_Init() .
uint8_t CAN_Init_TypeDef::phaseBufferSegment2 |
Default Phase Buffer Segment 2.
Definition at line
172
of file
em_can.h
.
Referenced by CAN_Init() .
uint8_t CAN_Init_TypeDef::propagationTimeSegment |
Default Propagation Time Segment.
Definition at line
166
of file
em_can.h
.
Referenced by CAN_Init() .
bool CAN_Init_TypeDef::resetMessages |
True to reset messages during initialization.
Definition at line
160
of file
em_can.h
.
Referenced by CAN_Init() .
uint8_t CAN_Init_TypeDef::synchronisationJumpWidth |
Default Synchronisation Jump Width.
Definition at line
175
of file
em_can.h
.
Referenced by CAN_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_can.h