LCD_Init_TypeDef Struct ReferenceEMLIB > LCD
LCD Controller Initialization structure.
Definition at line
272
of file
em_lcd.h
.
#include <
em_lcd.h
>
Data Fields |
|
| LCD_Bias_TypeDef | bias |
| LCD_ChargeRedistribution_TypeDef | chargeRedistribution |
| int | contrastLevel |
| bool | enable |
| uint8_t | frameRateDivider |
| LCD_Mode_Typedef | mode |
| LCD_Mux_TypeDef | mux |
| LCD_Wave_TypeDef | wave |
Field Documentation
| LCD_Bias_TypeDef LCD_Init_TypeDef::bias |
| bool LCD_Init_TypeDef::enable |
Enable controller at end of initialization.
Definition at line
274
of file
em_lcd.h
.
Referenced by LCD_Init() .
| LCD_Mode_Typedef LCD_Init_TypeDef::mode |
| LCD_Mux_TypeDef LCD_Init_TypeDef::mux |
| LCD_Wave_TypeDef LCD_Init_TypeDef::wave |
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_lcd.h