CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU

HFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.

Definition at line 2182 of file em_cmu.h .

#include < em_cmu.h >

Data Fields

uint16_t ctuneStartup
uint16_t ctuneSteadyState
CMU_OscMode_TypeDef mode
uint8_t timeoutPeakDetect
uint8_t timeoutStartup
uint8_t timeoutSteady
uint16_t xoCoreBiasTrimStartup
uint16_t xoCoreBiasTrimSteadyState

Field Documentation

uint16_t CMU_HFXOInit_TypeDef::ctuneStartup

Startup phase CTUNE (load capacitance) value

Definition at line 2184 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint16_t CMU_HFXOInit_TypeDef::ctuneSteadyState

Steady-state phase CTUNE (load capacitance) value

Definition at line 2185 of file em_cmu.h .

Referenced by BSP_initClocks() , and CMU_HFXOInit() .

CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode

Oscillator mode

Definition at line 2211 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::timeoutPeakDetect

Timeout - peak detection

Definition at line 2188 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::timeoutStartup

Timeout - startup

Definition at line 2190 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::timeoutSteady

Timeout - steady-state

Definition at line 2189 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint16_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup

Startup XO core bias current trim

Definition at line 2186 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint16_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState

Steady-state XO core bias current trim

Definition at line 2187 of file em_cmu.h .

Referenced by CMU_HFXOInit() .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/ em_cmu.h