VddCheckKit Drivers
Detailed Description
VDD Voltage Check using EMLIB Voltage Comparator (VCOMP) API.
Functions |
|
void | VDDCHECK_Disable (void) |
VCMP deinitialization routine.
|
|
void | VDDCHECK_Init (void) |
VCMP initialization routine.
|
|
bool | VDDCHECK_LowVoltage (float vdd) |
Check if voltage is higher than indicated.
|
|
Function Documentation
bool VDDCHECK_LowVoltage | ( | float |
vdd
|
) |
Check if voltage is higher than indicated.
- Parameters
-
vdd
The voltage level to compare against.
- Returns
- Returns true if voltage is lower, false otherwise
Definition at line
68
of file
vddcheck.c
.