MSDSCSI_ReadCapacity_TypeDef Struct ReferenceKit Drivers > Gecko USB MSD
SCSI Read Capacity Command Descriptor Block (CDB) typedef.
Definition at line
177
of file
msdscsi.h
.
#include <
msdscsi.h
>
Data Fields |
|
struct { | |
uint8_t Obsolete : 1 | |
uint8_t Reserved1 : 7 | |
}; | |
struct { | |
uint8_t Pmi : 1 | |
uint8_t Reserved3 : 7 | |
}; | |
uint8_t | Control |
uint32_t | Lba |
uint8_t | OpCode |
uint16_t | Reserved2 |
Field Documentation
uint8_t MSDSCSI_ReadCapacity_TypeDef::Control |
Control byte.
Definition at line
189
of file
msdscsi.h
.
uint32_t MSDSCSI_ReadCapacity_TypeDef::Lba |
Logical Block (sector) Address.
Definition at line
183
of file
msdscsi.h
.
uint8_t MSDSCSI_ReadCapacity_TypeDef::Obsolete |
Obsolete, expect any value.
Definition at line
180
of file
msdscsi.h
.
uint8_t MSDSCSI_ReadCapacity_TypeDef::OpCode |
Command opcode.
Definition at line
178
of file
msdscsi.h
.
uint8_t MSDSCSI_ReadCapacity_TypeDef::Pmi |
Partial medium indicator.
Definition at line
186
of file
msdscsi.h
.
uint8_t MSDSCSI_ReadCapacity_TypeDef::Reserved1 |
Reserved, expect 0.
Definition at line
181
of file
msdscsi.h
.
uint16_t MSDSCSI_ReadCapacity_TypeDef::Reserved2 |
Reserved, expect 0.
Definition at line
184
of file
msdscsi.h
.
uint8_t MSDSCSI_ReadCapacity_TypeDef::Reserved3 |
Reserved, expect 0.
Definition at line
187
of file
msdscsi.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/hardware/kit/common/drivers/
msdscsi.h