API_LayerEMDRV > EZRADIODRV
Detailed Description
EzRadio API Layer
.
         Enumerations | 
       |
| enum | 
         
          EZRADIO_ConfigRet_t
         
         {
          EZRADIO_CONFIG_SUCCESS , EZRADIO_CONFIG_NO_PATCH , EZRADIO_CONFIG_CTS_TIMEOUT , EZRADIO_CONFIG_PATCH_FAIL , EZRADIO_CONFIG_COMMAND_ERROR }  | 
       
         Functions | 
       |
| void | ezradio_change_state (uint8_t next_state1) | 
| EZRADIO_ConfigRet_t | ezradio_configuration_init (const uint8_t *pSetPropCmd) | 
| void | ezradio_ezconfig_check (uint16_t checksum, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_fifo_info (uint8_t fifo, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_fifo_info_fast_read (ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_fifo_info_fast_reset (uint8_t fifo) | 
| void | ezradio_frr_a_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_frr_b_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_frr_c_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_frr_d_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_func_info (ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_get_adc_reading (uint8_t adc_en, uint8_t adc_cfg, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_get_chip_status (uint8_t chip_clr_pend, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_get_chip_status_fast_clear (void) | 
| void | ezradio_get_chip_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_get_int_status (uint8_t ph_clr_pend, uint8_t modem_clr_pend, uint8_t chip_clr_pend, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_get_int_status_fast_clear (void) | 
| void | ezradio_get_int_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_get_modem_status (uint8_t modem_clr_pend, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_get_modem_status_fast_clear (void) | 
| void | ezradio_get_modem_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_get_packet_info (uint8_t field_number_mask, uint16_t len, int16_t diff_len, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_get_ph_status (uint8_t ph_clr_pend, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_get_ph_status_fast_clear (void) | 
| void | ezradio_get_ph_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_get_property (uint8_t group, uint8_t num_props, uint8_t start_prop, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_gpio_pin_cfg (uint8_t gpio0, uint8_t gpio1, uint8_t gpio2, uint8_t gpio3, uint8_t nirq, uint8_t sdo, uint8_t gen_config, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_gpio_pin_cfg_fast (ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_ircal (uint8_t searching_step_size, uint8_t searching_rssi_avg, uint8_t rx_chain_setting1, uint8_t rx_chain_setting2) | 
| void | ezradio_ircal_manual (uint8_t ircal_amp, uint8_t ircal_ph, ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_nop (void) | 
| void | ezradio_part_info (ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_power_up (uint8_t boot_options, uint8_t xtal_options, uint32_t xo_freq) | 
| void | ezradio_read_cmd_buff (ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_read_rx_fifo (uint8_t numbytes, uint8_t *prxdata) | 
| void | ezradio_request_device_state (ezradio_cmd_reply_t *ezradioReply) | 
| void | ezradio_reset (void) | 
| void | ezradio_rx_hop (uint8_t inte, uint8_t frac2, uint8_t frac1, uint8_t frac0, uint8_t vco_cnt1, uint8_t vco_cnt0) | 
| void | ezradio_set_property (uint8_t group, uint8_t num_props, uint8_t start_prop,...) | 
| void | ezradio_start_rx (uint8_t channel, uint8_t condition, uint16_t rx_len, uint8_t next_state1, uint8_t next_state2, uint8_t next_state3) | 
| void | ezradio_start_rx_fast (void) | 
| void | ezradio_start_tx (uint8_t channel, uint8_t condition, uint16_t tx_len) | 
| void | ezradio_start_tx_fast (void) | 
| void | ezradio_tx_hop (uint8_t inte, uint8_t frac2, uint8_t frac1, uint8_t frac0, uint8_t vco_cnt1, uint8_t vco_cnt0, uint8_t pll_settle_time1, uint8_t pll_settle_time0) | 
| void | ezradio_write_ezconfig_array (uint8_t numBytes, uint8_t *pEzConfigArray) | 
| void | ezradio_write_tx_fifo (uint8_t numbytes, uint8_t *pdata) | 
Enumeration Type Documentation
| enum EZRADIO_ConfigRet_t | 
EZRadio device configuration return values
        Definition at line
        
         46
        
        of file
        
         ezradio_api_lib.h
        
        .
       
Function Documentation
| void ezradio_change_state | ( | uint8_t | 
           
            next_state1
           
           | 
          ) | 
Issue a change state command to the radio.
- Parameters
 - 
         
[in] next_state1Next state.  
        Definition at line
        
         282
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
Referenced by ezradioStopDirectReceive() , ezradioStopDirectTransmit() , ezradioStopPn9() , and ezradioStopUnmodulatedCarrier() .
| EZRADIO_ConfigRet_t ezradio_configuration_init | ( | const uint8_t * | 
           
            pSetPropCmd
           
           | 
          ) | 
This function is used to load all properties and commands with a list of NULL terminated commands. Before this function ezradio_reset should be called.
- Parameters
 - 
         
[in] pSetPropCmdPointer to the configuration array.  
        Definition at line
        
         37
        
        of file
        
         ezradio_api_lib_add.c
        
        .
       
References ezradio_comm_SendCmdGetResp() , EZRADIO_CONFIG_COMMAND_ERROR , EZRADIO_CONFIG_CTS_TIMEOUT , EZRADIO_CONFIG_SUCCESS , ezradio_get_int_status() , ezradio_hal_NirqLevel() , and ezradio_write_ezconfig_array() .
Referenced by ezradioInit() .
| void ezradio_ezconfig_check | ( | uint16_t | 
           
            checksum,
           
           | 
         
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Validates the EZConfig array was written correctly.
- Parameters
 - 
         
[in] checksumChecksum value [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         127
        
        of file
        
         ezradio_api_lib_add.c
        
        .
       
References ezradio_comm_CtsWentHigh , and ezradio_comm_SendCmdGetResp() .
| void ezradio_fifo_info | ( | uint8_t | 
           
            fifo,
           
           | 
         
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Send the FIFO_INFO command to the radio. Optionally resets the TX/RX FIFO. Reads the radio response back into ezradioReply.
- Parameters
 - 
         
[in] fifoRX/TX FIFO reset flags. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         316
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
Referenced by ezradioResetTRxFifo() .
| void ezradio_fifo_info_fast_read | ( | ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
          ) | 
Reads RX/TX FIFO count space. Does NOT reset RX/TX FIFO
- Parameters
 - 
         
[out] ezradioReplyReply structure of the command.  
        Definition at line
        
         946
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_fifo_info_fast_reset | ( | uint8_t | 
           
            fifo
           
           | 
          ) | 
Resets the RX/TX FIFO. Does not read back anything from TX/RX FIFO
- Parameters
 - 
         
[in] fifoFIFO to be reset.  
        Definition at line
        
         930
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_frr_a_read | ( | uint8_t | 
           
            respByteCount,
           
           | 
         
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Reads the Fast Response Registers starting with A register into ezradioReply union.
- Parameters
 - 
         
[in] respByteCountNumber of Fast Response Registers to be read. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         436
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_ReadData() .
| void ezradio_frr_b_read | ( | uint8_t | 
           
            respByteCount,
           
           | 
         
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Reads the Fast Response Registers starting with B register into ezradioReply union.
- Parameters
 - 
         
[in] respByteCountNumber of Fast Response Registers to be read. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         460
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_ReadData() .
| void ezradio_frr_c_read | ( | uint8_t | 
           
            respByteCount,
           
           | 
         
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Reads the Fast Response Registers starting with C register into ezradioReply union.
- Parameters
 - 
         
[in] respByteCountNumber of Fast Response Registers to be read. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         484
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_ReadData() .
| void ezradio_frr_d_read | ( | uint8_t | 
           
            respByteCount,
           
           | 
         
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Reads the Fast Response Registers starting with D register into ezradioReply union.
- Parameters
 - 
         
[in] respByteCountNumber of Fast Response Registers to be read. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         508
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_ReadData() .
| void ezradio_func_info | ( | ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
          ) | 
Sends the FUNC_INFO command to the radio, then reads the resonse into ezradioReply union.
- Parameters
 - 
         
[out] ezradioReplyReply structure of the command.  
        Definition at line
        
         410
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_get_adc_reading | ( | uint8_t | 
           
            adc_en,
           
           | 
         
| uint8_t | 
           
            adc_cfg,
           
           | 
         ||
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Reads the ADC values from the radio into ezradioReply union.
- Parameters
 - 
         
[in] adc_enADC enable parameter. [in] adc_cfgADC configuration parameter. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         162
        
        of file
        
         ezradio_api_lib_add.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_get_chip_status | ( | uint8_t | 
           
            chip_clr_pend,
           
           | 
         
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Gets the Chip status flags. Optionally clears them.
- Parameters
 - 
         
[in] chip_clr_pendFlags to clear. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         648
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_get_chip_status_fast_clear | ( | void | 
           
           
           | 
          ) | 
Clear all Chip status flags. Does NOT read back interrupt flags
        Definition at line
        
         890
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_get_chip_status_fast_clear_read | ( | ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
          ) | 
Clear and read all Chip status flags.
- Parameters
 - 
         
[out] ezradioReplyReply structure of the command.  
        Definition at line
        
         906
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_get_int_status | ( | uint8_t | 
           
            ph_clr_pend,
           
           | 
         
| uint8_t | 
           
            modem_clr_pend,
           
           | 
         ||
| uint8_t | 
           
            chip_clr_pend,
           
           | 
         ||
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Get the Interrupt status/pending flags form the radio and clear flags if requested.
- Parameters
 - 
         
[in] ph_clr_pendPacket Handler pending flags clear. [in] modem_clr_pendModem Status pending flags clear. [in] chip_clr_pendChip State pending flags clear. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         169
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
Referenced by ezradio_configuration_init() , ezradioInit() , ezradioPluginManager() , ezradioStartDirectReceive() , ezradioStartDirectTransmit() , ezradioStartPn9() , and ezradioStartUnmodulatedCarrier() .
| void ezradio_get_int_status_fast_clear | ( | void | 
           
           
           | 
          ) | 
Clear all Interrupt status/pending flags. Does NOT read back interrupt flags
        Definition at line
        
         737
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_get_int_status_fast_clear_read | ( | ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
          ) | 
Clear and read all Interrupt status/pending flags
- Parameters
 - 
         
[out] ezradioReplyReply structure of the command.  
        Definition at line
        
         752
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_get_modem_status | ( | uint8_t | 
           
            modem_clr_pend,
           
           | 
         
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Gets the Modem status flags. Optionally clears them.
- Parameters
 - 
         
[in] modem_clr_pendFlags to clear. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         617
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_get_modem_status_fast_clear | ( | void | 
           
           
           | 
          ) | 
Clear all Modem status flags. Does NOT read back interrupt flags
        Definition at line
        
         846
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_get_modem_status_fast_clear_read | ( | ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
          ) | 
Clear and read all Modem status flags.
- Parameters
 - 
         
[out] ezradioReplyReply structure of the command.  
        Definition at line
        
         862
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_get_packet_info | ( | uint8_t | 
           
            field_number_mask,
           
           | 
         
| uint16_t | 
           
            len,
           
           | 
         ||
| int16_t | 
           
            diff_len,
           
           | 
         ||
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Receives information from the radio of the current packet. Optionally can be used to modify the Packet Handler properties during packet reception.
- Parameters
 - 
         
[in] field_number_maskPacket Field number mask value. [in] lenLength value. [in] diff_lenDifference length. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         677
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_get_ph_status | ( | uint8_t | 
           
            ph_clr_pend,
           
           | 
         
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Gets the Packet Handler status flags. Optionally clears them.
- Parameters
 - 
         
[in] ph_clr_pendFlags to clear. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         592
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_get_ph_status_fast_clear | ( | void | 
           
           
           | 
          ) | 
Clear all Packet Handler status flags. Does NOT read back interrupt flags
        Definition at line
        
         808
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_get_ph_status_fast_clear_read | ( | ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
          ) | 
Clear and read all Packet Handler status flags.
- Parameters
 - 
         
[out] ezradioReplyReply structure of the command.  
        Definition at line
        
         824
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_get_property | ( | uint8_t | 
           
            group,
           
           | 
         
| uint8_t | 
           
            num_props,
           
           | 
         ||
| uint8_t | 
           
            start_prop,
           
           | 
         ||
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Get property values from the radio. Reads them into ezradioReply union.
- Parameters
 - 
         
[in] groupProperty group number. [in] num_propsNumber of properties to be read. [in] start_propStarting sub-property number. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         366
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_gpio_pin_cfg | ( | uint8_t | 
           
            gpio0,
           
           | 
         
| uint8_t | 
           
            gpio1,
           
           | 
         ||
| uint8_t | 
           
            gpio2,
           
           | 
         ||
| uint8_t | 
           
            gpio3,
           
           | 
         ||
| uint8_t | 
           
            nirq,
           
           | 
         ||
| uint8_t | 
           
            sdo,
           
           | 
         ||
| uint8_t | 
           
            gen_config,
           
           | 
         ||
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Send GPIO pin config command to the radio and reads the answer into ezradioReply union.
- Parameters
 - 
         
[in] gpio0GPIO0 configuration. [in] gpio1GPIO1 configuration. [in] gpio2GPIO2 configuration. [in] gpio3GPIO3 configuration. [in] nirqNIRQ configuration. [in] sdoSDO configuration. [in] gen_configGeneral pin configuration. [out] ezradioReplyReply structure of the command.  
        Definition at line
        
         210
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_gpio_pin_cfg_fast | ( | ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
          ) | 
Reads back current GPIO pin configuration. Does NOT configure GPIO pins
- Parameters
 - 
         
[out] ezradioReplyReply structure of the command.  
        Definition at line
        
         781
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_ircal | ( | uint8_t | 
           
            searching_step_size,
           
           | 
         
| uint8_t | 
           
            searching_rssi_avg,
           
           | 
         ||
| uint8_t | 
           
            rx_chain_setting1,
           
           | 
         ||
| uint8_t | 
           
            rx_chain_setting2
           
           | 
         ||
| ) | 
Performs image rejection calibration. Completion can be monitored by polling CTS or waiting for CHIP_READY interrupt source.
- Parameters
 - 
         
[in] searching_step_size[in] searching_rssi_avg[in] rx_chain_setting1[in] rx_chain_setting2 
        Definition at line
        
         128
        
        of file
        
         ezradio_api_lib_add.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_ircal_manual | ( | uint8_t | 
           
            ircal_amp,
           
           | 
         
| uint8_t | 
           
            ircal_ph,
           
           | 
         ||
| ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
         ||
| ) | 
Image rejection calibration. Forces a specific value for IR calibration, and reads back calibration values from previous calibrations
- Parameters
 - 
         
[in] ircal_amp[in] ircal_ph[out] ezradioReplyReply structure of the command.  
        Definition at line
        
         149
        
        of file
        
         ezradio_api_lib_add.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_nop | ( | void | 
           
           
           | 
          ) | 
Sends NOP command to the radio. Can be used to maintain SPI communication.
        Definition at line
        
         299
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_part_info | ( | ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
          ) | 
This function sends the PART_INFO command to the radio and receives the answer into ezradioReply union.
- Parameters
 - 
         
[out] ezradioReplyReply structure of the command.  
        Definition at line
        
         85
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_power_up | ( | uint8_t | 
           
            boot_options,
           
           | 
         
| uint8_t | 
           
            xtal_options,
           
           | 
         ||
| uint32_t | 
           
            xo_freq
           
           | 
         ||
| ) | 
This function is used to initialize after power-up the radio chip. Before this function ezradio_reset should be called.
- Parameters
 - 
         
[in] boot_optionsBoot options input to the power up command. [in] xtal_optionsXTAL options input to the power up command. [in] xo_freqXO frequency input to the power up command.  
        Definition at line
        
         64
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_read_cmd_buff | ( | ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
          ) | 
Reads the command buffer
- Parameters
 - 
         
[out] ezradioReplyReply structure of the command.  
        Definition at line
        
         554
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
| void ezradio_read_rx_fifo | ( | uint8_t | 
           
            numBytes,
           
           | 
         
| uint8_t * | 
           
            pRxData
           
           | 
         ||
| ) | 
Reads the RX FIFO content from the radio.
- Parameters
 - 
         
[in] numBytesData length to be read. [in] pRxDataPointer to the buffer location.  
        Definition at line
        
         353
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_ReadData() .
| void ezradio_request_device_state | ( | ezradio_cmd_reply_t * | 
           
            ezradioReply
           
           | 
          ) | 
Requests the current state of the device and lists pending TX and RX requests.
- Parameters
 - 
         
[out] ezradioReplyReply structure of the command.  
        Definition at line
        
         531
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmdGetResp() .
Referenced by ezradioStartDirectTransmit() , ezradioStartPn9() , and ezradioStartUnmodulatedCarrier() .
| void ezradio_reset | ( | void | 
           
           
           | 
          ) | 
This functions is used to reset the EZRadio device by applying shutdown and releasing it. After this function ezradio_power_up or ezradio_configuration_init should be called. The user can check if POR has completed by waiting 4 ms or by polling radio GPIO 0, 2, or 3. When these GPIOs are high, it is safe to call the above mentioned functions.
        Definition at line
        
         38
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_ClearCTS() , ezradio_hal_AssertShutdown() , ezradio_hal_DeassertShutdown() , USTIMER_DeInit() , USTIMER_Delay() , and USTIMER_Init() .
| void ezradio_rx_hop | ( | uint8_t | 
           
            inte,
           
           | 
         
| uint8_t | 
           
            frac2,
           
           | 
         ||
| uint8_t | 
           
            frac1,
           
           | 
         ||
| uint8_t | 
           
            frac0,
           
           | 
         ||
| uint8_t | 
           
            vco_cnt1,
           
           | 
         ||
| uint8_t | 
           
            vco_cnt0
           
           | 
         ||
| ) | 
While in RX state this will hop to the frequency specified by the parameters and start searching for a preamble.
- Parameters
 - 
         
[in] intenew inte register value. [in] frac2new frac2 register value. [in] frac1new frac1 register value. [in] frac0new frac0 register value. [in] vco_cnt1new vco_cnt1 register value. [in] vco_cnt0new vco_cnt0 register value.  
        Definition at line
        
         209
        
        of file
        
         ezradio_api_lib_add.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_set_property | ( | uint8_t | 
           
            group,
           
           | 
         
| uint8_t | 
           
            num_props,
           
           | 
         ||
| uint8_t | 
           
            start_prop,
           
           | 
         ||
           
            ...
           
           | 
         |||
| ) | 
Send SET_PROPERTY command to the radio.
- Parameters
 - 
         
[in] groupProperty group. [in] num_propsNumber of property to be set. The properties must be in ascending order in their sub-property aspect. Max. 12 properties can be set in one command. [in] start_propStart sub-property address. [in] ...Variable number of properties to be set.  
        Definition at line
        
         253
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_start_rx | ( | uint8_t | 
           
            channel,
           
           | 
         
| uint8_t | 
           
            condition,
           
           | 
         ||
| uint16_t | 
           
            rx_len,
           
           | 
         ||
| uint8_t | 
           
            next_state1,
           
           | 
         ||
| uint8_t | 
           
            next_state2,
           
           | 
         ||
| uint8_t | 
           
            next_state3
           
           | 
         ||
| ) | 
Sends START_RX command to the radio.
- Parameters
 - 
         
[in] channelChannel number. [in] conditionStart RX condition. [in] rx_lenPayload length (exclude the PH generated CRC). [in] next_state1Next state when Preamble Timeout occurs. [in] next_state2Next state when a valid packet received. [in] next_state3Next state when invalid packet received (e.g. CRC error).  
        Definition at line
        
         144
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
Referenced by ezradioStartDirectReceive() , and ezradioStartRx() .
| void ezradio_start_rx_fast | ( | void | 
           
           
           | 
          ) | 
Sends START_RX command ID to the radio with no input parameters
        Definition at line
        
         723
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_start_tx | ( | uint8_t | 
           
            channel,
           
           | 
         
| uint8_t | 
           
            condition,
           
           | 
         ||
| uint16_t | 
           
            tx_len
           
           | 
         ||
| ) | 
Sends START_TX command to the radio.
- Parameters
 - 
         
[in] channelChannel number. [in] conditionStart TX condition. [in] tx_lenPayload length (exclude the PH generated CRC).  
        Definition at line
        
         115
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
Referenced by ezradioStartDirectTransmit() , ezradioStartPn9() , and ezradioStartUnmodulatedCarrier() .
| void ezradio_start_tx_fast | ( | void | 
           
           
           | 
          ) | 
Sends START_TX command ID to the radio with no input parameters
        Definition at line
        
         709
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_tx_hop | ( | uint8_t | 
           
            inte,
           
           | 
         
| uint8_t | 
           
            frac2,
           
           | 
         ||
| uint8_t | 
           
            frac1,
           
           | 
         ||
| uint8_t | 
           
            frac0,
           
           | 
         ||
| uint8_t | 
           
            vco_cnt1,
           
           | 
         ||
| uint8_t | 
           
            vco_cnt0,
           
           | 
         ||
| uint8_t | 
           
            pll_settle_time1,
           
           | 
         ||
| uint8_t | 
           
            pll_settle_time0
           
           | 
         ||
| ) | 
While in TX state this will hop to the frequency specified by the parameters
- Parameters
 - 
         
[in] intenew inte register value. [in] frac2new frac2 register value. [in] frac1new frac1 register value. [in] frac0new frac0 register value. [in] vco_cnt1new vco_cnt1 register value. [in] vco_cnt0new vco_cnt0 register value. [in] pll_settle_time1new pll_settle_time1 register value. [in] pll_settle_time0new pll_settle_time0 register value.  
        Definition at line
        
         181
        
        of file
        
         ezradio_api_lib_add.c
        
        .
       
References ezradio_comm_SendCmd() .
| void ezradio_write_ezconfig_array | ( | uint8_t | 
           
            numBytes,
           
           | 
         
| uint8_t * | 
           
            pEzConfigArray
           
           | 
         ||
| ) | 
Writes data byte(s) to the EZConfig array.
- Parameters
 - 
         
[in] numBytesnumber of bytes to send [in] pEzConfigArraypointer to the EZConfig configuration array  
        Definition at line
        
         116
        
        of file
        
         ezradio_api_lib_add.c
        
        .
       
References ezradio_comm_WriteData() .
Referenced by ezradio_configuration_init() .
| void ezradio_write_tx_fifo | ( | uint8_t | 
           
            numBytes,
           
           | 
         
| uint8_t * | 
           
            pTxData
           
           | 
         ||
| ) | 
The function can be used to load data into TX FIFO.
- Parameters
 - 
         
[in] numBytesData length to be load. [in] pTxDataPointer to the data (uint8_t*).  
        Definition at line
        
         342
        
        of file
        
         ezradio_api_lib.c
        
        .
       
References ezradio_comm_WriteData() .