BURTCEMLIB
Detailed Description
Backup Real Time Counter (BURTC) Peripheral API.
This module contains functions to control the BURTC peripheral of Silicon Labs 32-bit MCUs. The Backup Real Time Counter allows timekeeping in all energy modes. The Backup RTC is also available when the system is in backup mode.
         Data Structures | 
       |
| struct | BURTC_Init_TypeDef | 
         Macros | 
       |
| #define | BURTC_INIT_DEFAULT | 
| #define | burtcClkDiv_1 1 | 
| #define | burtcClkDiv_128 128 | 
| #define | burtcClkDiv_16 16 | 
| #define | burtcClkDiv_2 2 | 
| #define | burtcClkDiv_32 32 | 
| #define | burtcClkDiv_4 4 | 
| #define | burtcClkDiv_64 64 | 
| #define | burtcClkDiv_8 8 | 
         Enumerations | 
       |
| enum | 
         
          BURTC_ClkSel_TypeDef
         
         {
          burtcClkSelULFRCO = BURTC_CTRL_CLKSEL_ULFRCO, burtcClkSelLFRCO = BURTC_CTRL_CLKSEL_LFRCO, burtcClkSelLFXO = BURTC_CTRL_CLKSEL_LFXO }  | 
       
| enum | 
         
          BURTC_LP_TypeDef
         
         {
          burtcLPDisable = BURTC_LPMODE_LPMODE_DISABLE, burtcLPEnable = BURTC_LPMODE_LPMODE_ENABLE, burtcLPBU = BURTC_LPMODE_LPMODE_BUEN }  | 
       
| enum | 
         
          BURTC_Mode_TypeDef
         
         {
          burtcModeDisable = BURTC_CTRL_MODE_DISABLE, burtcModeEM2 = BURTC_CTRL_MODE_EM2EN, burtcModeEM3 = BURTC_CTRL_MODE_EM3EN, burtcModeEM4 = BURTC_CTRL_MODE_EM4EN }  | 
       
         Functions | 
       |
| uint32_t | BURTC_ClockFreqGet (void) | 
| 
         Get the clock frequency of the BURTC.
          | 
       |
| uint32_t | BURTC_CompareGet (unsigned int comp) | 
| 
         Get the BURTC compare value.
          | 
       |
| void | BURTC_CompareSet (unsigned int comp, uint32_t value) | 
| 
         Set BURTC compare channel.
          | 
       |
| __STATIC_INLINE uint32_t | BURTC_CounterGet (void) | 
| 
         Get BURTC counter.
          | 
       |
| void | BURTC_CounterReset (void) | 
| 
         Reset counter.
          | 
       |
| void | BURTC_Enable (bool enable) | 
| 
         Enable or Disable BURTC peripheral reset and start counter.
          | 
       |
| __STATIC_INLINE void | BURTC_FreezeEnable (bool enable) | 
| 
         Freeze register updates until enabled.
          | 
       |
| void | BURTC_Init (const BURTC_Init_TypeDef *burtcInit) | 
| 
         Initialize BURTC.
          | 
       |
| __STATIC_INLINE void | BURTC_IntClear (uint32_t flags) | 
| 
         Clear one or more pending BURTC interrupts.
          | 
       |
| __STATIC_INLINE void | BURTC_IntDisable (uint32_t flags) | 
| 
         Disable one or more BURTC interrupts.
          | 
       |
| __STATIC_INLINE void | BURTC_IntEnable (uint32_t flags) | 
| 
         Enable one or more BURTC interrupts.
          | 
       |
| __STATIC_INLINE uint32_t | BURTC_IntGet (void) | 
| 
         Get pending BURTC interrupt flags.
          | 
       |
| __STATIC_INLINE uint32_t | BURTC_IntGetEnabled (void) | 
| 
         Get enabled and pending BURTC interrupt flags.
          | 
       |
| __STATIC_INLINE void | BURTC_IntSet (uint32_t flags) | 
| 
         Set one or more pending BURTC interrupts from SW.
          | 
       |
| __STATIC_INLINE void | BURTC_Lock (void) | 
| 
         Lock BURTC registers, will protect from writing new config settings.
          | 
       |
| __STATIC_INLINE void | BURTC_Powerdown (bool enable) | 
| 
         Shut down power to rentention register bank.
          | 
       |
| void | BURTC_Reset (void) | 
| 
         Restore BURTC to reset state.
          | 
       |
| __STATIC_INLINE uint32_t | BURTC_RetRegGet (uint32_t num) | 
| 
         Read a value from one of the retention registers.
          | 
       |
| __STATIC_INLINE void | BURTC_RetRegSet (uint32_t num, uint32_t data) | 
| 
         Set a value in one of the retention registers.
          | 
       |
| __STATIC_INLINE uint32_t | BURTC_Status (void) | 
| 
         Status of BURTC RAM, timestamp and LP Mode.
          | 
       |
| __STATIC_INLINE void | BURTC_StatusClear (void) | 
| 
         Clear and reset BURTC status register.
          | 
       |
| __STATIC_INLINE void | BURTC_SyncWait (void) | 
| 
         Wait for the BURTC to complete all synchronization of register changes and commands.
          | 
       |
| __STATIC_INLINE uint32_t | BURTC_TimestampGet (void) | 
| 
         Get BURTC timestamp for entering BU.
          | 
       |
| __STATIC_INLINE void | BURTC_Unlock (void) | 
| 
         Unlock BURTC registers, enable write access to change configuration.
          | 
       |
Macro Definition Documentation
| #define BURTC_INIT_DEFAULT | 
Default configuration for BURTC initialization structure.
        Definition at line
        
         131
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_1 1 | 
BURTC clock divisors. These values are valid for the BURTC prescaler. Divide clock by 1.
        Definition at line
        
         61
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_128 128 | 
Divide clock by 128.
        Definition at line
        
         68
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_16 16 | 
Divide clock by 16.
        Definition at line
        
         65
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_2 2 | 
Divide clock by 2.
        Definition at line
        
         62
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_32 32 | 
Divide clock by 32.
        Definition at line
        
         66
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_4 4 | 
Divide clock by 4.
        Definition at line
        
         63
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_64 64 | 
Divide clock by 64.
        Definition at line
        
         67
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_8 8 | 
Divide clock by 8.
        Definition at line
        
         64
        
        of file
        
         em_burtc.h
        
        .
       
Enumeration Type Documentation
| enum BURTC_ClkSel_TypeDef | 
| enum BURTC_LP_TypeDef | 
| enum BURTC_Mode_TypeDef | 
Function Documentation
| uint32_t BURTC_ClockFreqGet | ( | void | 
           
           
           | 
          ) | 
Get the clock frequency of the BURTC.
- Returns
 - The current frequency in Hz.
 
Ultra-low frequency (1 kHz) clock.
Low-frequency RC oscillator.
Low-frequency crystal oscillator.
        Definition at line
        
         375
        
        of file
        
         em_burtc.c
        
        .
       
References _BURTC_CTRL_CLKSEL_MASK , _BURTC_CTRL_PRESC_DIV1 , _BURTC_CTRL_PRESC_MASK , _BURTC_CTRL_PRESC_SHIFT , BURTC , BURTC_CTRL_CLKSEL_LFRCO , BURTC_CTRL_CLKSEL_LFXO , BURTC_CTRL_CLKSEL_ULFRCO , SystemLFRCOClockGet() , SystemLFXOClockGet() , and SystemULFRCOClockGet() .
| uint32_t BURTC_CompareGet | ( | unsigned int | 
           
            comp
           
           | 
          ) | 
Get the BURTC compare value.
- Parameters
 - 
         
[in] compCompare the channel index value, must be 0 for Giant/Leopard Gecko.  
- Returns
 - The currently configured value for this compare channel.
 
        Definition at line
        
         301
        
        of file
        
         em_burtc.c
        
        .
       
References BURTC .
| void BURTC_CompareSet | ( | unsigned int | 
           
            comp,
           
           | 
         
| uint32_t | 
           
            value
           
           | 
         ||
| ) | 
Set BURTC compare channel.
- Parameters
 - 
         
[in] compCompare the channel index, must be 0 for current devices. [in] valueNew compare value.  
        Definition at line
        
         271
        
        of file
        
         em_burtc.c
        
        .
       
References BURTC , and BURTC_SYNCBUSY_COMP0 .
| __STATIC_INLINE uint32_t BURTC_CounterGet | ( | void | 
           
           
           | 
          ) | 
Get BURTC counter.
- Returns
 - BURTC counter value
 
        Definition at line
        
         373
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC .
| void BURTC_Enable | ( | bool | 
           
            enable
           
           | 
          ) | 
Enable or Disable BURTC peripheral reset and start counter.
- Parameters
 - 
         
[in] enableIf true; asserts reset to BURTC, halts counter, if false; deassert reset  
        Definition at line
        
         253
        
        of file
        
         em_burtc.c
        
        .
       
References _BURTC_CTRL_MODE_MASK , _BURTC_CTRL_RSTEN_SHIFT , BURTC , BURTC_CTRL_MODE_DISABLE , and BUS_RegBitWrite() .
Referenced by BURTC_Init() .
| __STATIC_INLINE void BURTC_FreezeEnable | ( | bool | 
           
            enable
           
           | 
          ) | 
Freeze register updates until enabled.
- Parameters
 - 
         
[in] enableIf true, registers are not updated until enabled again.  
        Definition at line
        
         394
        
        of file
        
         em_burtc.h
        
        .
       
References _BURTC_FREEZE_REGFREEZE_SHIFT , BURTC , and BUS_RegBitWrite() .
Referenced by BURTC_Init() .
| void BURTC_Init | ( | const BURTC_Init_TypeDef * | 
           
            burtcInit
           
           | 
          ) | 
Initialize BURTC.
Configures the BURTC peripheral.
- Note
 - 
         Before initialization, BURTC module must first be enabled by clearing the reset bit in the RMU, i.e.,
         
* RMU_ResetControl(rmuResetBU, rmuResetModeClear); *
Compare channel 0 must be configured outside this function, before initialization if enable is set to true. The counter will always be reset. 
- Parameters
 - 
         
[in] burtcInitA pointer to the BURTC initialization structure.  
        Definition at line
        
         129
        
        of file
        
         em_burtc.c
        
        .
       
References _BURTC_CTRL_BUMODETSEN_SHIFT , _BURTC_CTRL_COMP0TOP_SHIFT , _BURTC_CTRL_DEBUGRUN_SHIFT , _BURTC_CTRL_LPCOMP_SHIFT , _BURTC_CTRL_PRESC_SHIFT , BURTC , BURTC_CTRL_RSTEN , BURTC_Enable() , BURTC_FreezeEnable() , BURTC_IntClear() , BURTC_SYNCBUSY_LPMODE , BURTC_SyncWait() , burtcClkSelULFRCO , burtcLPDisable , burtcModeDisable , BURTC_Init_TypeDef::clkDiv , BURTC_Init_TypeDef::clkSel , BURTC_Init_TypeDef::compare0Top , BURTC_Init_TypeDef::debugRun , BURTC_Init_TypeDef::enable , BURTC_Init_TypeDef::lowPowerComp , BURTC_Init_TypeDef::lowPowerMode , BURTC_Init_TypeDef::mode , and BURTC_Init_TypeDef::timeStamp .
| __STATIC_INLINE void BURTC_IntClear | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Clear one or more pending BURTC interrupts.
- Parameters
 - 
         
[in] flagsBURTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).  
        Definition at line
        
         180
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC .
Referenced by BURTC_Init() .
| __STATIC_INLINE void BURTC_IntDisable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Disable one or more BURTC interrupts.
- Parameters
 - 
         
[in] flagsBURTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).  
        Definition at line
        
         198
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC .
| __STATIC_INLINE void BURTC_IntEnable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Enable one or more BURTC interrupts.
- Note
 - Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using BURTC_IntClear() prior to enabling if a pending interrupt should be ignored.
 
- Parameters
 - 
         
[in] flagsBURTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).  
        Definition at line
        
         221
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC .
| __STATIC_INLINE uint32_t BURTC_IntGet | ( | void | 
           
           
           | 
          ) | 
Get pending BURTC interrupt flags.
- Note
 - This function does not clear the event bits.
 
- Returns
 - Pending BURTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
 
        Definition at line
        
         241
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC .
| __STATIC_INLINE uint32_t BURTC_IntGetEnabled | ( | void | 
           
           
           | 
          ) | 
Get enabled and pending BURTC interrupt flags.
- Note
 - The event bits are not cleared by the use of this function.
 
- Returns
 - Pending BURTC interrupt sources that is also enabled. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
 
        Definition at line
        
         258
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC .
| __STATIC_INLINE void BURTC_IntSet | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Set one or more pending BURTC interrupts from SW.
- Parameters
 - 
         
[in] flagsBURTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).  
        Definition at line
        
         278
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC .
| __STATIC_INLINE void BURTC_Powerdown | ( | bool | 
           
            enable
           
           | 
          ) | 
Shut down power to rentention register bank.
- Parameters
 - 
         
[in] enableIf true, shuts off power to retention registers.  
- Note
 - When power rentention is disabled, it cannot be enabled again (until reset).
 
        Definition at line
        
         407
        
        of file
        
         em_burtc.h
        
        .
       
References _BURTC_POWERDOWN_RAM_SHIFT , BURTC , and BUS_RegBitWrite() .
| void BURTC_Reset | ( | void | 
           
           
           | 
          ) | 
Restore BURTC to reset state.
- Note
 - Before accessing the BURTC, BURSTEN in RMU->CTRL must be cleared. LOCK will not be reset to default value, as this will disable access to core BURTC registers.
 
        Definition at line
        
         337
        
        of file
        
         em_burtc.c
        
        .
       
References _BURTC_IEN_RESETVALUE , _BURTC_IF_MASK , _RMU_CTRL_BURSTEN_SHIFT , BURTC , BURTC_SyncWait() , BUS_RegBitRead() , BUS_RegBitWrite() , and RMU .
| __STATIC_INLINE uint32_t BURTC_RetRegGet | ( | uint32_t | 
           
            num
           
           | 
          ) | 
Read a value from one of the retention registers.
- Parameters
 - 
         
[in] numRetention Register to read  
        Definition at line
        
         435
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC .
| __STATIC_INLINE void BURTC_RetRegSet | ( | uint32_t | 
           
            num,
           
           | 
         
| uint32_t | 
           
            data
           
           | 
         ||
| ) | 
Set a value in one of the retention registers.
- Parameters
 - 
         
[in] numRegister to set [in] dataValue to put into register  
        Definition at line
        
         421
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC .
| __STATIC_INLINE uint32_t BURTC_Status | ( | void | 
           
           
           | 
          ) | 
Status of BURTC RAM, timestamp and LP Mode.
- Returns
 - A mask logially OR-ed status bits
 
        Definition at line
        
         293
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC .
| __STATIC_INLINE uint32_t BURTC_TimestampGet | ( | void | 
           
           
           | 
          ) | 
Get BURTC timestamp for entering BU.
- Returns
 - BURTC Time Stamp value
 
        Definition at line
        
         385
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC .