VCMP_Init_TypeDef Struct ReferenceEMLIB > VCMP
VCMP Initialization structure.
       Definition at line
       
        93
       
       of file
       
        em_vcmp.h
       
       .
      
      
       #include <
       
     
        em_vcmp.h
       
       >
      
         Data Fields | 
       |
| int | biasProg | 
| bool | enable | 
| bool | halfBias | 
| VCMP_Hysteresis_TypeDef | hyst | 
| int | inactive | 
| bool | irqFalling | 
| bool | irqRising | 
| bool | lowPowerRef | 
| int | triggerLevel | 
| VCMP_WarmTime_TypeDef | warmup | 
Field Documentation
| int VCMP_Init_TypeDef::biasProg | 
BIAS current configuration, depends on Half Bias setting above, see reference manual for more information.
        Definition at line
        
         98
        
        of file
        
         em_vcmp.h
        
        .
       
Referenced by VCMP_Init() .
| bool VCMP_Init_TypeDef::enable | 
Enable VCMP after configuration.
        Definition at line
        
         115
        
        of file
        
         em_vcmp.h
        
        .
       
Referenced by VCMP_Init() , and VDDCHECK_LowVoltage() .
| bool VCMP_Init_TypeDef::halfBias | 
If set to true, reduces the bias current by half.
        Definition at line
        
         95
        
        of file
        
         em_vcmp.h
        
        .
       
Referenced by VCMP_Init() .
| VCMP_Hysteresis_TypeDef VCMP_Init_TypeDef::hyst | 
| int VCMP_Init_TypeDef::inactive | 
Output value when comparator is inactive, should be 0 or 1.
        Definition at line
        
         108
        
        of file
        
         em_vcmp.h
        
        .
       
Referenced by VCMP_Init() .
| bool VCMP_Init_TypeDef::irqFalling | 
Enable interrupt for falling edge.
        Definition at line
        
         100
        
        of file
        
         em_vcmp.h
        
        .
       
Referenced by VCMP_Init() .
| bool VCMP_Init_TypeDef::irqRising | 
Enable interrupt for rising edge.
        Definition at line
        
         102
        
        of file
        
         em_vcmp.h
        
        .
       
Referenced by VCMP_Init() .
| bool VCMP_Init_TypeDef::lowPowerRef | 
Enable low power mode for VDD and band gap reference.
        Definition at line
        
         110
        
        of file
        
         em_vcmp.h
        
        .
       
Referenced by VCMP_Init() , and VDDCHECK_LowVoltage() .
| int VCMP_Init_TypeDef::triggerLevel | 
Trigger level, according to formula: VDD Trigger Level = 1.667V + 0.034V x triggerLevel
        Definition at line
        
         113
        
        of file
        
         em_vcmp.h
        
        .
       
Referenced by VCMP_Init() , and VDDCHECK_LowVoltage() .
| VCMP_WarmTime_TypeDef VCMP_Init_TypeDef::warmup | 
Warm-up time in clock cycles.
        Definition at line
        
         104
        
        of file
        
         em_vcmp.h
        
        .
       
Referenced by VCMP_Init() , and VDDCHECK_LowVoltage() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/platform/emlib/inc/
       
em_vcmp.h