ADC_InitSingle_TypeDef Struct ReferenceEMLIB > ADC
Single conversion initialization structure.
Definition at line 964
of file em_adc.h
.
#include <
em_adc.h
>
Data Fields | |
ADC_AcqTime_TypeDef | acqTime |
bool | diff |
ADC_SingleInput_TypeDef | input |
bool | leftAdjust |
bool | prsEnable |
ADC_PRSSEL_TypeDef | prsSel |
ADC_Ref_TypeDef | reference |
bool | rep |
ADC_Res_TypeDef | resolution |
Field Documentation
ADC_AcqTime_TypeDef ADC_InitSingle_TypeDef::acqTime |
Acquisition time (in ADC clock cycles).
Definition at line 972
of file em_adc.h
.
Referenced by ADC0_IRQHandler(), ADC_InitSingle(), and adcInit().
bool ADC_InitSingle_TypeDef::diff |
Select if single-ended or differential input.
Definition at line 1003
of file em_adc.h
.
Referenced by ADC_InitSingle().
ADC_SingleInput_TypeDef ADC_InitSingle_TypeDef::input |
Sample input selection, use single-ended or differential input according to setting of diff
.
Definition at line 988
of file em_adc.h
.
Referenced by ADC0_IRQHandler(), ADC_InitSingle(), and TOUCH_Init().
bool ADC_InitSingle_TypeDef::leftAdjust |
Select if left adjustment should be done.
Definition at line 1009
of file em_adc.h
.
Referenced by ADC_InitSingle().
bool ADC_InitSingle_TypeDef::prsEnable |
Peripheral reflex system trigger enable.
Definition at line 1006
of file em_adc.h
.
Referenced by ADC_InitSingle(), and adcInit().
ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if prsEnable
is enabled.
Definition at line 969
of file em_adc.h
.
Referenced by ADC_InitSingle(), and adcInit().
ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference |
Sample reference selection. Note that, for external references, the ADC calibration register must be set explicitly.
Definition at line 978
of file em_adc.h
.
Referenced by ADC0_IRQHandler(), ADC_InitSingle(), adcInit(), and TOUCH_Init().
bool ADC_InitSingle_TypeDef::rep |
Select if continuous conversion until explicit stop.
Definition at line 1012
of file em_adc.h
.
Referenced by ADC_InitSingle().
ADC_Res_TypeDef ADC_InitSingle_TypeDef::resolution |
Sample resolution.
Definition at line 981
of file em_adc.h
.
Referenced by ADC0_IRQHandler(), ADC_InitSingle(), and TOUCH_Init().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emlib/inc/
em_adc.h