CHAR_TypeDef Struct ReferenceKit Drivers > SegmentLcd
Defines each text symbol's segment in terms of COM and BIT numbers, in a way that we can enumerate each bit for each text segment in the following bit pattern:
* -------0------ * * | \7 |8 /9 | * |5 \ | / |1 * * --6--- ---10-- * * | / | \11 | * |4 /13 |12 \ |2 * * -------3------ *
E.g.: First text character bit pattern #3 (above) is Segment 1D for Display Location COM 3, BIT 0
       Definition at line
       
        83
       
       of file
       
        segmentlcd.c
       
       .
      
         Data Fields | 
       |
| uint8_t | bit [14] | 
| uint8_t | com [14] | 
Field Documentation
| uint8_t CHAR_TypeDef::bit[14] | 
| uint8_t CHAR_TypeDef::com[14] | 
LCD COM line (for multiplexing)
        Definition at line
        
         84
        
        of file
        
         segmentlcd.c
        
        .
       
Referenced by SegmentLCD_Write() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/hardware/kit/common/drivers/
       
segmentlcd.c