VCMPEMLIB
Detailed Description
Voltage Comparator (VCMP) Peripheral API.
This module contains functions to control the VCMP peripheral of Silicon Labs 32-bit MCUs and SoCs. The VCMP monitors the input voltage supply and generates interrupts on events using as little as 100 nA.
         Data Structures | 
       |
| struct | VCMP_Init_TypeDef | 
         Macros | 
       |
| #define | VCMP_INIT_DEFAULT | 
         Enumerations | 
       |
| enum | 
         
          VCMP_Hysteresis_TypeDef
         
         {
          vcmpHystNone , vcmpHyst20mV }  | 
       
| enum | 
         
          VCMP_WarmTime_TypeDef
         
         {
          vcmpWarmTime4Cycles = _VCMP_CTRL_WARMTIME_4CYCLES, vcmpWarmTime8Cycles = _VCMP_CTRL_WARMTIME_8CYCLES, vcmpWarmTime16Cycles = _VCMP_CTRL_WARMTIME_16CYCLES, vcmpWarmTime32Cycles = _VCMP_CTRL_WARMTIME_32CYCLES, vcmpWarmTime64Cycles = _VCMP_CTRL_WARMTIME_64CYCLES, vcmpWarmTime128Cycles = _VCMP_CTRL_WARMTIME_128CYCLES, vcmpWarmTime256Cycles = _VCMP_CTRL_WARMTIME_256CYCLES, vcmpWarmTime512Cycles = _VCMP_CTRL_WARMTIME_512CYCLES }  | 
       
         Functions | 
       |
| __STATIC_INLINE void | VCMP_Disable (void) | 
| 
         Disable Voltage Comparator.
          | 
       |
| __STATIC_INLINE void | VCMP_Enable (void) | 
| 
         Enable Voltage Comparator.
          | 
       |
| void | VCMP_Init (const VCMP_Init_TypeDef *vcmpInit) | 
| 
         Configure and enable Voltage Comparator.
          | 
       |
| __STATIC_INLINE void | VCMP_IntClear (uint32_t flags) | 
| 
         Clear one or more pending VCMP interrupts.
          | 
       |
| __STATIC_INLINE void | VCMP_IntDisable (uint32_t flags) | 
| 
         Disable one or more VCMP interrupts.
          | 
       |
| __STATIC_INLINE void | VCMP_IntEnable (uint32_t flags) | 
| 
         Enable one or more VCMP interrupts.
          | 
       |
| __STATIC_INLINE uint32_t | VCMP_IntGet (void) | 
| 
         Get pending VCMP interrupt flags.
          | 
       |
| __STATIC_INLINE uint32_t | VCMP_IntGetEnabled (void) | 
| 
         Get enabled and pending VCMP interrupt flags.
          | 
       |
| __STATIC_INLINE void | VCMP_IntSet (uint32_t flags) | 
| 
         Set one or more pending VCMP interrupts from SW.
          | 
       |
| void | VCMP_LowPowerRefSet (bool enable) | 
| 
         Enable or disable Low Power Reference setting.
          | 
       |
| __STATIC_INLINE bool | VCMP_Ready (void) | 
| 
         VCMP output is ready.
          | 
       |
| void | VCMP_TriggerSet (int level) | 
| 
         Configure the trigger level of the voltage comparator.
          | 
       |
| __STATIC_INLINE bool | VCMP_VDDHigher (void) | 
| 
         Returns true if Voltage Comparator indicated VDD > trigger level, else returns false.
          | 
       |
| __STATIC_INLINE bool | VCMP_VDDLower (void) | 
| 
         Returns true if Voltage Comparator indicated VDD < trigger level, else returns false.
          | 
       |
| __STATIC_INLINE uint32_t | VCMP_VoltageToLevel (float v) | 
| 
         Calculate voltage to trigger level.
          | 
       |
Macro Definition Documentation
| #define VCMP_INIT_DEFAULT | 
Default VCMP initialization structure.
        Definition at line
        
         119
        
        of file
        
         em_vcmp.h
        
        .
       
Referenced by VDDCHECK_LowVoltage() .
Enumeration Type Documentation
Warm-up Time in High Frequency Peripheral Clock cycles.
        Definition at line
        
         60
        
        of file
        
         em_vcmp.h
        
        .
       
Function Documentation
| void VCMP_Init | ( | const VCMP_Init_TypeDef * | 
           
            vcmpInit
           
           | 
          ) | 
Configure and enable Voltage Comparator.
- Parameters
 - 
         
[in] vcmpInitThe VCMP Initialization structure.  
        Definition at line
        
         59
        
        of file
        
         em_vcmp.c
        
        .
       
References _VCMP_CTRL_BIASPROG_MASK , _VCMP_CTRL_BIASPROG_SHIFT , _VCMP_CTRL_INACTVAL_SHIFT , _VCMP_CTRL_WARMTIME_MASK , _VCMP_CTRL_WARMTIME_SHIFT , VCMP_Init_TypeDef::biasProg , VCMP_Init_TypeDef::enable , VCMP_Init_TypeDef::halfBias , VCMP_Init_TypeDef::hyst , VCMP_Init_TypeDef::inactive , VCMP_Init_TypeDef::irqFalling , VCMP_Init_TypeDef::irqRising , VCMP_Init_TypeDef::lowPowerRef , VCMP_Init_TypeDef::triggerLevel , VCMP , VCMP_CTRL_EN , VCMP_CTRL_HALFBIAS , VCMP_CTRL_HYSTEN , VCMP_CTRL_IFALL , VCMP_CTRL_IRISE , VCMP_IF_EDGE , VCMP_IntClear() , VCMP_LowPowerRefSet() , VCMP_Ready() , VCMP_TriggerSet() , vcmpHyst20mV , vcmpHystNone , and VCMP_Init_TypeDef::warmup .
Referenced by VDDCHECK_LowVoltage() .
| __STATIC_INLINE void VCMP_IntClear | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Clear one or more pending VCMP interrupts.
- Parameters
 - 
         
[in] flagsVCMP interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).  
        Definition at line
        
         224
        
        of file
        
         em_vcmp.h
        
        .
       
References VCMP .
Referenced by VCMP_Init() .
| __STATIC_INLINE void VCMP_IntDisable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Disable one or more VCMP interrupts.
- Parameters
 - 
         
[in] flagsVCMP interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).  
        Definition at line
        
         252
        
        of file
        
         em_vcmp.h
        
        .
       
References VCMP .
| __STATIC_INLINE void VCMP_IntEnable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Enable one or more VCMP interrupts.
- Parameters
 - 
         
[in] flagsVCMP interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).  
        Definition at line
        
         266
        
        of file
        
         em_vcmp.h
        
        .
       
References VCMP .
| __STATIC_INLINE uint32_t VCMP_IntGet | ( | void | 
           
           
           | 
          ) | 
Get pending VCMP interrupt flags.
- Note
 - The event bits are not cleared by the use of this function.
 
- Returns
 - Pending VCMP interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the VCMP module (VCMP_IFS_nnn).
 
        Definition at line
        
         282
        
        of file
        
         em_vcmp.h
        
        .
       
References VCMP .
| __STATIC_INLINE uint32_t VCMP_IntGetEnabled | ( | void | 
           
           
           | 
          ) | 
Get enabled and pending VCMP interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
 - The event bits are not cleared by the use of this function.
 
- Returns
 - 
         Pending and enabled VCMP interrupt sources. The return value is the bitwise AND combination of
         
- the OR combination of enabled interrupt sources in VCMP_IEN_nnn register (VCMP_IEN_nnn) and
 - the OR combination of valid interrupt flags of the VCMP module (VCMP_IF_nnn).
 
 
        Definition at line
        
         305
        
        of file
        
         em_vcmp.h
        
        .
       
References VCMP .
| __STATIC_INLINE void VCMP_IntSet | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Set one or more pending VCMP interrupts from SW.
- Parameters
 - 
         
[in] flagsVCMP interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).  
        Definition at line
        
         238
        
        of file
        
         em_vcmp.h
        
        .
       
References VCMP .
| void VCMP_LowPowerRefSet | ( | bool | 
           
            enable
           
           | 
          ) | 
Enable or disable Low Power Reference setting.
- Parameters
 - 
         
[in] enableIf true, enables low power reference. If false, disable low power reference.  
        Definition at line
        
         139
        
        of file
        
         em_vcmp.c
        
        .
       
References VCMP , and VCMP_INPUTSEL_LPREF .
Referenced by VCMP_Init() .
| void VCMP_TriggerSet | ( | int | 
           
            level
           
           | 
          ) | 
Configure the trigger level of the voltage comparator.
- Parameters
 - 
         
[in] levelA trigger value, in range 0-63.  
        Definition at line
        
         155
        
        of file
        
         em_vcmp.c
        
        .
       
References _VCMP_INPUTSEL_TRIGLEVEL_MASK , _VCMP_INPUTSEL_TRIGLEVEL_SHIFT , and VCMP .
Referenced by VCMP_Init() .
| __STATIC_INLINE uint32_t VCMP_VoltageToLevel | ( | float | 
           
            v
           
           | 
          ) | 
Calculate voltage to trigger level.
- Note
 - Soft float support is needed for this function to work.
 
- Parameters
 - 
         
[in] vVoltage Level for trigger.  
        Definition at line
        
         169
        
        of file
        
         em_vcmp.h
        
        .
       
Referenced by VDDCHECK_LowVoltage() .