LESENSE_PerCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
LESENSE peripheral control descriptor structure.
       Definition at line
       
        566
       
       of file
       
        em_lesense.h
       
       .
      
      
       #include <
       
     
        em_lesense.h
       
       >
      
Field Documentation
| LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp0Mode | 
Configure how LESENSE controls ACMP 0.
        Definition at line
        
         606
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp1Mode | 
Configure how LESENSE controls ACMP 1.
        Definition at line
        
         609
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ControlDACConv_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0ConvMode | 
Configure how LESENSE controls conversion on DAC channel 0.
        Definition at line
        
         572
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0Data | 
Configure DAC channel 0 data control.
        Definition at line
        
         568
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ControlDACOut_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0OutMode | 
Configure how LESENSE controls output on DAC channel 0.
        Definition at line
        
         577
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ControlDACConv_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1ConvMode | 
Configure how LESENSE controls conversion on DAC channel 1.
        Definition at line
        
         585
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1Data | 
Configure DAC channel 1 data control.
        Definition at line
        
         581
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ControlDACOut_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1OutMode | 
Configure how LESENSE controls output on DAC channel 1.
        Definition at line
        
         590
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| uint8_t LESENSE_PerCtrlDesc_TypeDef::dacPresc | 
Configure the prescaling factor for the LESENSE - DAC interface. Valid range: 0-31 (5-bit).
        Definition at line
        
         596
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_DACRef_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacRef | 
Configure the DAC reference to be used. Set to lesenseDACRefVdd to use VDD and set to lesenseDACRefBandGap to use band gap as reference.
        Definition at line
        
         602
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_WarmupMode_TypeDef LESENSE_PerCtrlDesc_TypeDef::warmupMode | 
Configure how LESENSE controls ACMPs and DAC in idle mode.
        Definition at line
        
         612
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/platform/emlib/inc/
       
em_lesense.h