EZRADIODRV_PacketTxHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Transmit_Plugin

EzRadio transmit plug-in instance initialization and handler structure.

Definition at line 85 of file ezradio_transmit_plugin.h.

#include <ezradio_transmit_plugin.h>

Data Fields

uint8_t channel
 Transmission channel.
 
EZRADIODRV_PacketLengthConfig_t lenConfig
 Packet length configuration.
 
uint16_t pktId
 Packet ID.
 
EZRADIODRV_TransmitPacketType_t pktType
 Packet type.
 
EZRADIODRV_Callback_t userCallback
 User callback.
 

The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emdrv/ezradiodrv/plugins/inc/ezradio_transmit_plugin.h